DUG_AC Fan controller_CLP-00

Example of an automation

This demonstration shows you how to create an automation to turn on the fan when outdoor temperature exceeds certain value.
  1. Go to Automation > + to create an automation.
  2. Tap Edit name , enter the name of the automation and tap Save.
    TIP: You can choose the cover image that represents your automation by tapping .
  3. Tap Add Condition > When weather changes > Outdoor Temperature, set temperature (A) and then tap Next.
  4. Tap Run the device > Iconic Fan Controller > Fan Speed and select a function and then tap Save > Next.
  5. In the Automation Settings page, tap Save.

    Automation is now available under Automation tab. Use toggle switch to enable/disable automation.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.