DUG_AC Fan controller_CLP-00

Changing the Mode

Using mode setting, timer can be set to turn off the device after a set period of time or you can set it as a switch to turn on/off manually.

On the Settings page, tap Mode and select any of the following:

Switch: control the speed and turn on/off of the fan.

Timer: when fan is running, set the timer to turn off. Refer using mode timer.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.