DUG_Wiser Micro Module Dimmer_CLP-00

Adjusting the brightness level using app

Using the Wiser app , you can increase/decrease the brightness level remotely.
To increase/decrease the brightness level:
  1. On the Home page, tap All devices.
  2. In Micromodule Dimmer tap the power button (A) to turn on/off the device.

  3. Tap for slide-up menu.
  4. In the slide-up menu, drag the sliding bar (B) to increase/decrease the brightness.

  5. Alternatively, you can navigate to device menu and tap on (C) to turn on/off the device. When the device is turned on, drag the sliding bar (D) up/down to increase/decrease the brightness.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.