DUG_Iconic Connected Switch 10AX_CLP-00

About the device

Iconic Connected Switch 10AX offers reliable, resistant and flexible installation options and is ideal for controlling lighting and exhaust fans.
It can be controlled through the push button on the wall, remotely using the Wiser by SE app, with default Zigbee mode it can connect to the Wiser Hub for full home control and automation functions, point to point using Bluetooth Low Energy (BLE).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.