DUG_Iconic Connected Twin 10 A Socket_CLP-00

About the device

The Iconic Connected Socket Twin 10 A (hereinafter referred as Iconic Socket) is a connected electrical outlet designed to manage and control electrical devices in a convenient and efficient manner. It provides app controlled switching of plug-in appliances using the Wiser by SE app.
In BLE mode, the socket has a 12-24 hr time delay and 24/7 schedule functionality. In Zigbee mode, the socket can be integrated into Moments and Automations or simply be operated with time-scheduled output. When the manual switch on the socket is in the smart position, the socket can be controlled remotely.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.