DUG_Iconic Connected Twin 10 A Socket_CLP-00

Changing device protocol

The communication protocol of the device can be changed from Zigbee® to Bluetooth® and Bluetooth® to Zigbee®.

To change the pairing mode:

Short press the touch button 3 times and then long press once (> 30s).

Bluetooth pairing mode changes to Zigbee pairing mode, or Zigbee pairing mode changes to Bluetooth pairing mode.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.