DUG_Iconic Connected Twin 10 A Socket_CLP-00

Switching on/off the device using app

By using the Wiser app, you can switch on/off the device.
NOTE: Using the Wiser app, you can only operate the socket remotely if the rocker switch is in a smart state.
  1. In home page, next to device name, tap the ˅ for common function.
  2. Select the left/right socket (A).
  3. Tap the power button (B) to switch on/off.
    TIP: You can also navigate to the control panel of the device and tap to switch on/off the socket .
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.