DUG_Iconic Connected Twin 10 A Socket_CLP-00

Setting timer mode

You can set the timer to turn off the device after a certain period of time.
In Wiser app, change the mode from switch to timer, refer to mode settings
  1. On the device control panel page, tap timer (A) for the slide-up menu.
  2. In the slide-up menu select the required Set Period (B) and tap Save.
Once the countdown timer reaches zero, the device turns off.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.