DUG_Wiser Micro Module Blind_CLP-00

About the device

The Wiser Micro Module Blind (hereinafter referred to as module) combines the advantages of smart shutter functionality with ordinary mechanical double push-button switches. It transforms a conventional switch into a connected device that you can control from the switch or through the Wiser app.
Relay contacts are mechanically locked against each other to prevent simultaneous triggering of the two relay outputs.
NOTE: Do not control any devices that depend on a permanent power supply.

Additional features:

  • Remote control with maximum of 10 mechanical double push-button switches.

  • Protection of the motor against damage with two mutually mechanically and electronically locked relay contacts.

  • Electronic overload protection, overheating protection and short-circuit protection.

  • Setting a time schedule.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.