DUG_Wiser Micro Module Blind_CLP-00

For your safety

DANGER
Hazard of electric shock, explosion, or arc flash
Safe electrical installation must be carried out only by skilled professionals. Skilled professionals must prove profound knowledge in the following areas:
  • Connecting to installation networks.
  • Connecting several electrical devices.
  • Laying electric cables.
  • Safety standards, local wiring rules and regulations.
Failure to follow these instructions will result in death or serious injury.
DANGER
hazard of electric shock
  • Make sure that the terminal connection area does not come in contact with the metallic parts of any device installed in the same location.
  • Do not short the outputs to neutral.
  • The motor contacts and live conductor connection must be separated from one another by a 240 VAC basic insulation.
Failure to follow these instructions will result in death or serious injury.
WARNING
HAZARD OF ELECTRIC SHOCK
  • Observe the regulations for working on live parts.
  • Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.