DUG_Wiser Micro Module Blind_CLP-00

Resetting the device

You can reset the device to factory default manually.
Short press the push button 3 times and then long press the push button once for 10 s.
After 10 s, LED starts blinking red then release the operation button.
NOTE: All configuration data, user data, and network data are deleted. After which
  • No connectivity to other devices or rooms

  • No timer settings

The LED stops blinking upon successful reset of the device.
The module restarts and blinks green for a few seconds.
NOTE: After reset, the LED turns orange indicating that the device is ready for pairing.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.