DUG_Wiser Micro Module Dimmer_CLP-00

Removing the device

Using the Wiser app , you can remove a device from the device list.
To remove the device:
  1. On the Home page, tap All devices > Micromodule Dimmer.
  2. Tap to display more details.
  3. Tap Remove and Factory Reset Device (A).

    TIP: On the Home page, tap and hold the Micromodule Dimmer to remove the device.
    NOTE:
    • Removing the device will reset the module. After reset the LED turns orange indicating that the module is ready to pair with another network.

    • If there is a problem while pairing or resetting the module, refer to Resetting the device manually.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.