DUG_Wiser Micro Module Dimmer_CLP-00

Resetting the device

You can reset the device to factory default manually.
  1. Short press the push button 3 times and then long press the push button once for 10 s.

  2. After 10 s, LED starts blinking red, then release the push-button.
    NOTE: All configuration data, user data, and network data are deleted. After which
    • No connectivity to other devices or rooms.

    • Memory function is active.

    • Automatic load detection is active, RC mode is set.

    • Dimmer settings will reset to default.

    The LED stops blinking upon successful reset of the device.
    The module restarts and blinks green for a few seconds.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.