DUG_Wiser Micro Module Dimmer_CLP-00

Toggle mode setting

You can toggle between the last used brightness level or with 100% brightness level when the dimmer is turned on.
To toggle between the brightness level:
  1. On the Home page, tap All devices > Micromodule Dimmer.
  2. Tap Settings.
  3. Tap Toggle Mode Setting and select either one of the function for default action.
    • 100% (A) : to set the brightness level to 100% by default when ever the device is turned on.
    • Last Level (B) : to set the previously used brightness level by default when ever the device is turned on.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.