DUG_Smoke alarm AC Square_CLP-00

Testing the device

The device has a test mode that helps ensure the proper operation of the device. It is recommended to test the device once a month. If the device is installed in a mobile home, it is recommended to test the device weekly and before every journey.

NOTE: Using Wiser app you can set the monthly reminder for test alarm in settings.

Testing the individual device

IMPORTANT: Test the device once a month to ensure proper operation.

Press the Test/Hush button on each device for more than 3 s until an alarm sounds off. If the test alarm does not sound, then the device is not connected to power supply.


Testing the interconnected device(s)

It is possible to test all the devices simultaneously in an interconnected network with one operation.

  1. Select any interconnected device.

  2. Press and hold the Test/Hush button for more than 18 s until an alarm goes off on all interconnected devices.

If there is no alarm triggered on the interconnected devices, make sure that the wireless interconnection setup is correct. Also the distance between each device is within the specification.

NOTE: The triggered alarm on the interconnected devices remains for a longer time even if you release the Test/Hush button.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.