DUG_Window/Door Sensor_CLP-00

Example of an automation

This demonstration shows you how to create an automation to switch on the light when the door is opened.
  1. Go to Automation > + to create an automation.
  2. Tap Edit name , enter the name of the automation and tap Save.
    TIP: You can choose the cover image that represents your automation by tapping .
  3. Tap Add Condition > When device status changes > Window/Door Sensor.
  4. Tap Window/Door Sensor > Open.
  5. Tap Add task > Run the device and select Micro Module Light Switch.
  6. Tap Switch > On (A) and tap Save.
  7. Tap Next.

  8. In the Automation Settings page, tap Save.

    Once the automation is saved, it is visible on the Automation tab. You can tap the toggle switch on the automation to enable it.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.