DUG_IPC_Indoor_CLP–02

Configuring basic function settings

Using the Wiser app, you can configure the following features:

Flip screen

Enabling the Flip screen will turn the screen upside down on the live view on control panel.

Follow the steps to enable the Flip screen:

  1. On the Home page, tap All devices > IP Camera Indoor.

  2. Tap and tap Settings > Basic function settings.

  3. Tap the toggle switch (A) to enable the Flip screen.

Time watermark

Enabling the Time watermark displays the date and time on the live view on control panel.

Follow the steps to enable the Time watermark:

  1. On the Home page, tap All devices > IP Camera Indoor.

  2. Tap and tap Settings > Basic function settings.

  3. Tap the toggle switch (B) to enable the Time watermark.

Talk mode

Using the Talk mode, you can make one-way or two-way communication with the receiver.

Tap Talk mode (C) and select one of the options:

– One-Way Communication - Tap and hold to send a voice message, the other party can receive it and then reply to you with a voice message

– Two-Way Intercom - You and the other party can talk at the same time

Camera calibration

You can use Camera calibration feature to check if the camera is covering wider angle of the view.

Tap Camera calibration (D) and confirm the calibration process.

NOTE: The IP camera will turn automatically during the process. It might take 25 seconds to do the calibration.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.