DUG_IPC_Indoor_CLP–02

Using the device

Using the control panel of the IP Camera, you can see live video of the indoors on the display screen and includes the following features:
TIP: LED blinks green on the device indicating that the IP Camera is in use.

Enables audio of the live video

Makes the video fullscreen

Moves the camera in four directions (up, down, right, left)

Takes screenshot of the live view

Lets you communicate with a person near the device

Records the live view

NOTE:
  • To view the saved screenshot/recording, tap > Album.

  • To view the notification/alarm messages, tap > Message.

  • To review the recordings using playback feature, refer to Playback.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.