DUG_IPC_Indoor_CLP–02

Creating a moment

A Moment allows you to group multiple actions that are usually done together. Using the Wiser app, you can create moments based on your needs (such as movie night).
Follow the steps to create a moment:
  1. On the Home page, tap .
  2. Go to Moment > + to create a moment.
  3. Tap Edit name, enter the name of the moment (A) and tap Save.
    TIP: You can choose the cover image that best represents your moment by tapping .

  4. In the Action section, tap Add task (B) to open the slide-up menu.
  5. In the Add task menu, you can do either or all of the following actions (C):
    • Run the device - Select the devices that you want in a moment
    • Select Automation - Select the automation that you want to enable or disable. For more info refer to Automation
    • Delay - Set the delay time
    NOTE: You can add one or more actions using .

  6. Tap Run the device > IP Camera Indoor to select either or all of the functions to add in the moment:
    • Private Mode - Turn on/off the private mode (D)
    • Recording - Turn on/off the recording (E)
    • Mode - Select the type of recording (F)
    • Auto-patrol Switch - Turn on/off the patrol mode (G)

  7. Once all the actions are set, tap Save.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.