DUG_IPC_Indoor_CLP–02

Troubleshooting

Symptom

Possible cause

Solution

The device is not ready to pair after the device is removed from the app.

The device is not reset correctly.

Long press the reset button for 3 seconds located on the back of the device to reset the device.

The device does not respond.

Wrong Wi-Fi credentials are entered during the pairing process.

NOTE: You must log into 2.4 GHz network.

The Wiser IP Camera Indoor cannot connect to the internet via the Wi-Fi network router.

The router port settings may not be properly set for system access to the internet.

Check that the following router ports are open:

  • Port 6667

  • Port 6666

  • Port 6668

  • Port 6669

  • Port 1883

  • Port 8886

  • Port 8883

  • Port 443

IMPORTANT: For cyber-security, check that all unused ports are closed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.