DOCA0186EN-02

NSX Cord

DANGER
hazard of electric shock, explosion or arc flash
  • It is forbidden to use the NSX cords LV434200, LV434201, or LV434202 if the system voltage is greater than 480 Vac or 480 Vdc.
  • It is mandatory to use the insulated NSX cord LV434204 if the system voltage is greater than 480 Vac or 480 Vdc, and less than or equal to 690 Vac or 690 Vdc.
Failure to follow these instructions will result in death or serious injury.

Introduction

The NSX cord connects a circuit breaker to the communication network.

The NSX cord can be used with a BSCM Modbus SL/ULP module module.

NOTE: The NSX cord cannot be installed in a ComPacT NSX DC EP circuit breaker.

For more information about integrating ComPacT NSX DC circuit breaker communication functions, refer to:

  • DOCA0093EN ULP System (IEC Standard) - User Guide

  • DOCA0213EN ComPacT NSX - Modbus Communication Guide

Description

The NSX cord consists of a junction box, a cable equipped with an RJ45 connector, and a cable equipped with a screw terminal block.

Item

Data medium

Data transmitted

Comments

A

NSX cord microswitch

State of SD contact

The NSX cord goes into the SD slot instead of the auxiliary contact.

B

Cable equipped with an RJ45 connector for connection to a ULP module.

Communication network

Three cable lengths are available: 0.3 m (9.84 ft), 1.3 m (4.27 ft), and 3 m (14.7 ft).

C

Internal link to the BSCM Modbus SL/ULP module

Communication network

The NSX cord also provides the 24 Vdc power supply for the BSCM Modbus SL/ULP module (when this module is installed):

Installation

The slots used to install the NSX cord depend on the circuit breaker type.

ComPacT NSX100-250 DC 3P/4P

ComPacT NSX400-630 DC 3P/4P

ComPacT NSX1200 DC 2P

A NSX cord

B BSCM Modbus SL/ULP module

The NSX cord cannot be installed at the same time as the SD auxiliary contact.

The NSX cord can be installed on site.

For more information about installation, consult the instruction sheet on the Schneider Electric website: GHD16047AA ComPacT NSX100–630 – NSX cord.

NSX Cord Connection

The NSX cord connects to the following ULP modules:

  • IFM or IFE communication interface

  • FDM121 display

  • IO module

The figure below illustrates the connections from the NSX cord to the IFM Modbus interface.

A IFM Modbus interface for one circuit breaker

B NSX cord

C BSCM Modbus SL/ULP module

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.