DOCA0186EN-02

Operating the Circuit Breakers

Circuit Breaker Operating Control Accessories for General-Purpose Applications

The following table shows the operating control accessories compatible with the ComPacT NSX DC circuit breakers for general-purpose applications. For more information, refer to LVPED221002EN ComPacT NSX, ComPacT INS/INV, MasterPacT NW DC - DC PV Catalog.

Operating Control Accessory

NSX100 DC

NSX160 DC

NSX250 DC

NSX400 DC

NSX630 DC

NSX1200 DC

1P

2P

3P/4P

1P

2P

3P/4P

3P/4P

3P/4P

3P/4P

2P

Toggle handle

✔ ✔ ✔ ✔ ✔ ✔ ✔ ✔ ✔ ✔

Rotary handle

– – ✔ – – ✔ ✔ ✔ ✔ ✔

Motor mechanism

– – ✔ – – ✔ ✔ ✔ ✔ ✔

Communicating motor mechanism

– – ✔ – – ✔ ✔ ✔ ✔ ✔

Circuit Breaker Operating Control Accessories for Photovoltaic and Marine Applications

The following table shows the operating control accessories compatible with the ComPacT NSX DC PV and DC EP circuit breakers for photovoltaic and marine applications. For more information, refer to LVPED221002EN ComPacT NSX, ComPacT INS/INV, MasterPacT NW DC - DC PV Catalog.

Operating Control Accessory

NSX80-200
DC PV

NSX400-500
DC PV

NSX100-250
DC EP

NSX250-500
DC EP

4P

4P

4P

4P

Toggle handle

✔ ✔ ✔ ✔

Rotary handle

✔ ✔ ✔ ✔

Motor mechanism

✔ ✔ - -

Communicating motor mechanism

✔ ✔ - -

Handle Position

The handle position indicates the state of the circuit breaker:

Toggle handle

Rotary handle

Motor mechanism

  • I (ON): Circuit breaker closed.

    Closed manually.

  • O (OFF): Circuit breaker open.

    Opened manually.

  • Trip: Circuit breaker tripped.

    Tripped by the protection (trip unit or trip auxiliaries), the push-to-trip button, or the USB maintenance interface.

  • I (ON): Circuit breaker closed (in Auto or Manu mode).

  • O (OFF): Circuit breaker open or tripped (in Auto or Manu mode).

Remote Indication

Information is available remotely:

  • From the indication contacts

  • From the wireless indication auxiliaries

  • By using a communication network

These indication auxiliaries can be installed on site.

For more information about the remote indication and communication options, refer to the summary tables of auxiliaries.

Remote Electrical Stop Command

The remote electrical stop command can be given by electrical control auxiliaries regardless of the control type in use.

To obtain a remote electrical stop command, use:

  • an MX shunt trip release, or

  • an MN undervoltage trip release, or

  • an MN undervoltage trip release with time-delay unit (the time-delay unit overcomes the problem of micro-cuts).

For more information about the electrical control auxiliaries, refer to the relevant topic.

NOTE: It is advisable to test operation of the remote electrical stop commands at regular intervals (every six months).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.