DOCA0186EN-02

TM-G Thermal-Magnetic Trip Unit for 3P and 4P Circuit Breakers up to 250 A

Introduction

The TM-G thermal-magnetic trip unit for 3P/4P circuit breakers up to 250 A are interchangeable trip units.

They are designed for DC general-purpose applications.

The TM-G interchangeable 3P/4P trip units provide:

  • adjustable thermal threshold

  • fixed magnetic pick-up

Description

The adjustment dial is on the front of the trip unit.

A Setting range for the TM-G thermal-magnetic trip unit

B Adjustment dial for the thermal protection pick-up Ir

Setting the Thermal Protection

The thermal protection pick-up Ir is set by a 4-setting dial.

Turning the thermal protection adjustment dial (A) modifies the trip curve as shown (B).

The following table shows the values of the pick-up Ir (in amperes) for thermal protection (values indicated on the dial) with respect to every trip unit rating, relative to the position of the dial Ir.

Trip Unit Rating In (A)

16

25

40

63

80

100

125

160

200

250

Pick-up Ir (A)

11

18

28

44

56

70

88

112

140

175

13

20

32

50

64

80

100

128

160

200

14

23

36

57

72

90

113

144

180

225

16

25

40

63

80

100

125

160

200

250

Setting the Magnetic Protection

The magnetic protection pick-up cannot be adjusted and equals the value shown below:

 

Trip Unit Rating In (A)

16

25

40

63

80

100

125

160

200

250

Fixed Pick-up Ii (A) +/– 20%

AC value

63

80

80

125

200

320

440

440

440

520

DC value

80

100

100

150

240

380

530

530

530

620

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.