DOCA0186EN-02

Trip Unit Summary

General-Purpose Applications

The following table shows the trip units compatible with the ComPacT NSX DC circuit breakers for general-purpose applications. For further details, refer to LVPED221002EN ComPacT NSX, ComPacT INS/INV, MasterPacT NW DC - DC PV Catalog.

Trip Units

Built-in / Interchangeable

NSX100
DC

NSX160
DC

NSX250
DC

NSX400
DC

NSX630
DC

NSX1200
DC

1P

2P

3P/4P

1P

2P

3P/4P

3P/4P

3P/4P

3P/4P

2P

NA (switch-disconnector)

Built-in

– – – – – – – ✔ ✔ –

NA (switch-disconnector)

Interchangeable

– – ✔ – – ✔ ✔ – – –

TM-D

Built-in

✔ ✔ – ✔ ✔ – – – – –

TM-D

Interchangeable

– – ✔ – – ✔ – – – –

TM-DC

Built-in

– – – – – – – ✔ ✔ ✔

TM-DC

Interchangeable

– – ✔ – – ✔ ✔ – – –

TM-G

Interchangeable

– – ✔ – – ✔ ✔ – – –

Photovoltaic and Marine Applications

The following tables shows the trip units compatible with the ComPacT NSX DC circuit breakers for photovoltaic and marine applications. For further details, refer to LVPED221002EN ComPacT NSX, ComPacT INS/INV, MasterPacT NW DC - DC PV Catalog

ComPacT NSX DC PV 4P Circuit Breakers

Trip Units

Built-in / Interchangeable

NSX80
DC PV

NSX100
DC PV

NSX125
DC PV

NSX160
DC PV

NSX200
DC PV

NSX400
DC PV

NSX500
DC PV

NA (switch-disconnector)

Built-in

– ✔ – ✔ ✔ ✔ ✔

TM-DC PV

Built-in

✔ – ✔ ✔ ✔ ✔ ✔

ComPacT NSX DC EP 4P Circuit Breakers

    NSX100–250 DC EP NSX250_630 DC EP

Trip Units

Built-in / Interchangeable

NSX100
DC EP

NSX125
DC EP

NSX160
DC EP

NSX200
DC EP

NSX250
DC EP

NSX250
DC EP

NSX320
DC EP

NSX400
DC EP

NSX500
DC EP

NSX630
DC EP

NA (switch-disconnector)

Built-in

✔ – ✔ ✔ ✔ – ✔ ✔ ✔ ✔

TM-DC EP

Built-in

✔ ✔ ✔ – ✔ ✔ ✔ ✔ ✔ –

Protections and Settings of Thermal-Magnetic Trip Units

The adjustment dials are on the front of the trip units.

A Overload protection threshold

B Short-circuit protection pick-up

Upgradability of Thermal-Magnetic Trip Units

Interchangeable trip units are upgradable. See tables above for more information on interchangeable trip units.

Onsite swapping of interchangeable trip units is simple and reliable:

  • No connections to make

  • No special tools (for example, calibrated torque wrench)

  • Compatibility of trip units ensured by mechanical cap

  • Torque limited screw ensures proper mounting (see drawing below)

The design of the trip units limits the risk of incorrect tightening or oversights. The simplicity of the swapping process means that it is easy to make the necessary adjustments as operation and maintenance processes evolve.

NOTE: When the trip unit has been mounted by this means, the trip unit can still be removed: the screw head is accessible.

Sealing the Protection

The transparent cover on thermal-magnetic trip units can be sealed to prevent modification of the protection settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.