DOCA0140EN-03

Thermal-Magnetic Trip Unit Summary

Introduction

Thermal-magnetic trip units are designed to provide protection for distribution or for specific applications.

Identification

Type of protection

TM-D

Thermal-magnetic trip unit

TM-G

Thermal-magnetic trip unit with low pickup (for protecting generators, very long feeds)

MA

Magnetic-only trip unit (for example, for protecting motors, transformers)

The following table shows the trip units compatible with the ComPact NSX circuit breakers. For more information, refer to LVPED217032EN, ComPact NSX & NSXm Catalogue.

Trip units

Built-in / Interchangeable

NSX100

NSX160

NSX250

NSX400

NSX630

1P

2P

3P/4P

1P

2P

3P/4P

1P

3P/4P

3P/4P

3P/4P

NA (switch-disconnector)

Built-in

–

–

–

–

–

–

–

–

✔

✔

TM-D

Built-in

✔

✔

–

✔

✔

–

✔

–

–

–

TM-D

Interchangeable

–

–

✔

–

–

✔

–

–

–

–

TM-AC

Built-in

–

–

–

–

–

–

–

–

✔

✔

TM-AC

Interchangeable

–

–

✔

–

–

✔

–

✔

–

–

TM-G

Interchangeable

–

–

✔

–

–

✔

–

✔

–

–

MA

Interchangeable

–

–

✔

–

–

✔

–

✔

–

–

Protections and Settings of Thermal-Magnetic Trip Units

The adjustment dials are on the front of the trip units:

Item

Parameter

Description

Type(1)

TM-D

TM-G

MA

A

–

Trip unit setting range: minimum setting/maximum setting.

Trip unit rating In corresponds to the maximum value of the setting range.

O

O

O

B

Ir

Thermal protection pickup

✔

✔

–

C

tr

Thermal protection time delay

O

O

–

D

Ii

Magnetic protection pickup

✔/O

O

✔

E

–

Magnetic protection time delay

O

O

O

(1) Functions:

✔: Adjustable

O: Non-adjustable

✔/O: Adjustable or non-adjustable according to the trip unit rating

–: Not present

Upgradeability of Thermal-Magnetic Trip Units

WARNING
HAZARD OF DESTRUCTION OF THE MICROLOGIC TRIP UNIT
It is mandatory to use snap-off screws LV429513 to install a MicroLogic trip unit.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Upgradeability of trip units depends on the circuit breaker type:

  • For 1 or 2 poles, trip units are built-in.

  • For 3 or 4 poles, trip units are interchangeable.

NOTE: In ComPact NSX circuit breakers with R, HB1, HB2, and K breaking performances, the trip units are not interchangeable.

Onsite swapping of trip units is simple and reliable:

  • No connections to make

  • No specific tools (for example, calibrated torque wrench)

  • Compatibility of trip units provided by mechanical cap

  • Torque limited screw provides proper mounting (see drawing below)

The design of the trip units limits the risk of incorrect tightening or oversights. The simplicity of the swapping process means that it is easy to make the necessary adjustments as operation and maintenance processes evolve.

NOTE: When the trip unit has been mounted by this means, the trip unit can still be removed: the screw head is accessible. When a trip unit is reinstalled after being removed, it is mandatory to use torque limiting snap-off screws LV429513 for the reinstallation.

Sealing the Protection

The transparent cover on thermal-magnetic trip units can be sealed to prevent modification of the protection settings:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.