DOCA0091EN-08

Earth-Leakage Test History

General Description

The earth-leakage test history registers describe the last 10 earth-leakage tests performed on a MicroLogic 7 trip unit. The earth-leakage test history format corresponds to a series of 10 records. Each record is composed of 5 registers describing one earth-leakage test.

The earth-leakage test history registers return 32768 (0x8000) when they are not used.

Earth-Leakage Test Number

A read request of 5 x n registers is necessary to read the last n earth-leakage test records, where 5 is the number of registers for each earth-leakage test record.

For example, a read request of 5 x 2 = 10 registers is necessary to read the last 2 earth-leakage test records of the earth-leakage test history:

  • The first 5 registers describe the first earth-leakage test record (most recent earth-leakage test).

  • The last 5 registers describe the second earth-leakage test record.

Address

Register

Description

0x7593–0x7597

30100-30104

Earth-leakage test record (most recent earth-leakage test)

0x7598–0x759C

30105–30109

Earth-leakage test record 2

0x759D–0x75A1

30110–30114

Earth-leakage test record 3

0x75A2–0x75A6

30115–30119

Earth-leakage test record 4

0x75A7–0x75AB

30120–30124

Earth-leakage test record 5

0x75AC–0x75B0

30125–30129

Earth-leakage test record 6

0x75B1–0x75B5

30130–30134

Earth-leakage test record 7

0x75B6–0x75BA

30135–30139

Earth-leakage test record 8

0x75BB–0x75BF

30140–30144

Earth-leakage test record 9

0x75C0–0x75C4

30145–30149

Earth-leakage test record 10 (oldest earth-leakage test)

Earth-Leakage Test Record

A read request of 5 registers is necessary to read a earth-leakage test record.

The order and the description of the earth-leakage test record registers are the same as that of the earth-leakage test record 1:

Earth-Leakage Test Record 1 (Most Recent Earth-Leakage Test)

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x7593

30100

R

1

–

INT16U

0–65535

E

Earth-leakage test code (see next section.)

0x7594–

0x7596

30101–

30103

R

–

–

ULP DATE

–

E

Date and time of earth-leakage test. Data Type: ULP DATE

0x7597

30104

R

–

–

INT16U

0–1

E

Test status

  • 0: test succeeded

  • 1: test failed

Earth-Leakage Test Codes

Earth-Leakage Test Code

Description

5162 (0x142A)

Earth-leakage test by button

5163 (0x142B)

Earth-leakage test by HMI