DOCA0091EN-08

Generic Commands

Change Output State

The command is used to change the state of IO module digital outputs assigned as user-defined outputs using the EcoStruxure Power Commission software.

To change the output state, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

–

INT16U

1672

Command code = 1672

0x1F40

8001

–

INT16U

13

Number of parameters (bytes) = 13

0x1F41

8002

–

INT16U

–

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

–

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

–

OCTET STRING

–

Password of the command: Administrator or Operator user profile password

0x1F45

8006

–

INT16U

1–3

Output number

  • 1 = output 1

  • 2 = output 2

  • 3 = output 3

0x1F46

8007

–

INT16U

–

Value to set:

  • 0x0000 = Change output state to 0 (OFF)

  • 0x0100 = Change output state to 1 (ON)

Reset IO Module Alarm

The alarms can be read from the alarm status register.

To reset IO module alarms, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

–

INT16U

41099

Command code = 41099

0x1F40

8001

–

INT16U

10

Number of parameters (bytes) = 10

0x1F41

8002

–

INT16U

–

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

–

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

–

OCTET STRING

–

Password of the command: Administrator or Operator user profile password

Enable/Disable Simple Commands

To enable or disable the simple commands, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

–

INT16U

41100

Command code = 41100

0x1F40

8001

–

INT16U

11

Number of parameters (bytes) = 11

0x1F41

8002

–

INT16U

–

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

–

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

–

OCTET STRING

–

Password of the command: Administrator or Operator user profile password

0x1F45

8006

–

INT16U

–

MSB: Enable or disable:

  • 0 = Disable simple command

  • 1 = Enable simple command

LSB: 0 (not used)

Acknowledge Latched Output

To acknowledge the latched output, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

–

INT16U

41102

Command code = 41102

0x1F40

8001

–

INT16U

11

Number of parameters (bytes) = 11

0x1F41

8002

–

INT16U

–

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

–

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

–

OCTET STRING

–

Password of the command: Administrator or Operator user profile password

0x1F45

8006

–

INT16U

–

MSB:

  • 0x01 = Digital output relay 1

  • 0x02 = Digital output relay 2

  • 0x03 = Digital output relay 3

  • 0xFF = Unlatch all digital output

LSB: 0 (not used)

Reset Analog Input Minimum/Maximum Values

The analog input maximum and minimum values can be read from the analog input registers.

To reset the minimum/maximum analog input values, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

–

INT16U

42890

Command code = 42890

0x1F40

8001

–

INT16U

10

Number of parameters (bytes) = 10

0x1F41

8002

–

INT16U

–

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

–

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

–

OCTET STRING

–

Password of the command: Administrator or Operator user profile password