DOCA0091EN-08

Applications

IO Application Status

Address

Register

RW

Unit

Type

Range

Bit

Description

0x3927

14632

R

–

INT16U

–

0

Cradle application enabled or disabled:

  • 0 = Disabled

  • 1 = Enabled

1–15

Reserved

0x3928

14633

R

–

INT16U

–

–

Quality of each bit of register 14632:

  • 0 = Invalid

  • 1 = Valid

Cradle Management

The table describes the registers related to the cradle management application performed by IO 1 (predefined or user defined application).

The registers 18300–18329 are related to the cradle management application performed by IO 2 (predefined or user defined application).

Address

Register

RW

Unit

Type

Range

Bit

Description

0x3BC3

15300

R-RC

–

INT16U

–

–

Quality of each bit of register 15301:

  • 0 = Invalid

  • 1 = Valid

0x3BC4

15301

R-RC

–

INT16U

–

–

Cradle status

0–7

Reserved

8

Device in disconnected position (CD)

9

Device in connected position (CE)

10

Device in the test position (CT)

11–15

Reserved

0x3BC5–0x3BC6

15302–15303

R-RC-WC

–

INT32U

0–65534

–

Cradle connected position counter

This counter increments for each rising edge of the cradle connected position

0x3BC7–0x3BC8

15304–15305

R-RC-WC

–

INT32U

0–65534

–

Cradle disconnected position counter

This counter increments for each rising edge of the cradle disconnected position

0x3BC9–0x3BCA

15306–15307

R-RC-WC

–

INT32U

0–65534

–

Cradle test position counter

This counter increments for each rising edge of the cradle test position

0x3BCB–0x3BCE

15308–15311

R-RC

–

DATETIME

–

–

Timestamp of the last change for the cradle connected position

0x3BCF–0x3BD2

15312–15315

R-RC

–

DATETIME

–

–

Timestamp of the last change for the cradle disconnected position

0x3BD3–0x3BD6

15316–15319

R-RC

–

DATETIME

–

–

Timestamp of the last change for the cradle test position

0x3BD7–0x3BD8

15320–15321

R-WC

s

INT32U

–

–

Operating time since last grease maintenance

0x3BD9–0x3BDA

15322–15323

R-WC

s

INT32U

–

–

Operating time since last move connected position

0x3BDB

15324

R

–

INT16U

0-65534

–

Cradle contact regrease counter

0x3BDC–0x3BE0

15325–15329

–

–

–

–

–

Reserved

Drawer Management

The table describes the registers related to the Drawer management user-defined application performed by IO 1.

The registers 18330–18359 are related to the Drawer management user-defined application performed by IO 2.

Address

Register

RW

Unit

Type

Range

Bit

Description

0x3BE1

15330

R

–

INT16U

–

–

Quality of each bit of register 15331:

0 = Invalid

1 = Valid

0x3BE2

15331

R

–

INT16U

–

–

Drawer status

0–7

Reserved

8

Drawer in disconnected position

9

Drawer in connected position

10

Drawer in the test position

11–15

Reserved

0x3BE3–0x3BE4

15332–15333

R

–

INT32U

–

–

Drawer connected position counter.

This counter increments for each rising edge of the drawer connected position.

0x3BE5–0x3BE6

15334–15335

R

–

INT32U

–

–

Drawer disconnected position counter.

This counter increments for each rising edge of the drawer disconnected position.

0x3BE7–0x3BE8

15336–15337

R

–

INT32U

–

–

Drawer test position counter.

This counter increments for each rising edge of the drawer test position.

0x3BE9–0x3BEC

15338–15341

R

–

DATETIME

–

–

Timestamp of the last change for the drawer connected position.

0x3BED–0x3BF0

15342–15345

R

–

DATETIME

–

–

Timestamp of the last change for the drawer disconnected position.

0x3BF1–0x3BF4

15346–15349

R

–

DATETIME

–

–

Timestamp of the last change for the drawer test position.

0x3BF5–0x3BFE

15350–15359

–

–

–

–

–

Reserved

Light Control

The table describes the registers related to the Light control predefined application performed by IO 1.

The registers 18400–18409 are related to the Light control predefined application performed by IO 2.

Address

Register

RW

Unit

Type

Range

Description

0x3C27

15400

R

–

INT16U

0–1

Quality of register 15401:

  • 0 = Invalid

  • 1 = Valid (application is configured and running)

0x3C28

15401

R

–

INT16U

0–1

Light status:

  • 0 = Reset/OFF

  • 1 = Set/ON

0x3C29–0x3C2A

15402–15403

R

s

INT32U

0–54000

Remaining time in ON or OFF state (depending of the light status)

0x3C2B–

15404

R

–

INT16U

0–2

Light simple command(1):

  • 0 = No command

  • 1 = Light OFF

  • 2 = Light ON

0x3C2C–0x3C30

15405–15409

–

–

–

–

Reserved

(1) Simple commands are enabled by factory setting. The simple commands can be disabled by using the command Enable/Disable simple commands.

Load Control

The table describes the registers related to the Load control predefined application performed by IO 1.

The registers 18410–18419 are related to the Load control predefined application performed by IO 2.

Address

Register

RW

Unit

Type

Range

Description

0x3C31

15410

R

–

INT16U

0–1

Quality of register 15411:

  • 0 = Invalid

  • 1 = Valid (application is configured and running)

0x3C32

15411

R

–

INT16U

0–1

Load status:

  • 0 = Reset/OFF

  • 1 = Set/ON

0x3C33–0x3C34

15412–15413

R

s

INT32U

0–54000

Remaining time in ON or OFF state (depending of the load status)

0x3C35

15414

R

–

INT16U

0–2

Load simple command(1):

  • 0 = No command

  • 1 = Load OFF

  • 2 = Load ON

0x3C36–

0x3EEC

15415–

16109

–

–

–

–

Reserved

(1) Simple commands are enabled by factory setting. The simple commands can be disabled by using the command Enable/Disable simple commands.