DOCA0091EN-08

Maintenance Indicators

Time of Use Counter

The time of use counter reports the time of use of the circuit breaker. The time of use is written in the EEPROM every hour. If the time of use counter reaches the maximum value 4 294 967 295 and a new time of use event occurs, then the counter is reset to 0.

A read request of 2 registers is necessary to read the time of use counter.

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x749A–0x749B

29851–29852

R

1

Hour

INT32U

0–4 294 967 295

A/E

Time of use counter

Rate of Wear Counter

The rate of wear counter reports the percentage of the circuit breaker contact use.

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x749C

29853

R

1

%

INT16U

0–32766

A/E

Rate of wear contact

0% = The circuit breaker contact is new.

> 100% = The circuit breaker contact must be changed.

Boot Counter

The boot counter reports the number of cold starts (power-up) and the number of warm starts (software reset of the MicroLogic trip unit).

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x749D

29854

R

1

–

INT16U

0–32766

A/E

Boot counter

EEPROM Writing Counter

The EEPROM writing counter reports the number of storages of the energy measurement in the EEPROM. The energy measurement is written in the EEPROM every hour. If the EEPROM writing counter reaches the maximum value 4 294 967 295 and a new EEPROM writing event occurs, then the EEPROM writing counter is reset to 0.

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x749E–

0x749F

29855–

29856

R

1

–

INT32U

0–4 294 967 295

A/E

Counter of EEPROM writing

Load Profile Counters

The load profile counters report the number of hours for each range of current in the MicroLogic trip unit. If the load profile counters reach the maximum value 4 294 967 295 and a new load profile event occurs, then the load profile counters are reset to 0.

A read request of 8 registers is necessary to read the load profile counters.

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x74B7–

0x74B8

29880–

29881

R

1

Hour

INT32U

0–4 294 967 295

A/E

Hours current was 0‑49% of nominal range

0x74B9–

0x74BA

29882–

29883

R

1

Hour

INT32U

0–4 294 967 295

A/E

Hours current was 50‑79% of nominal range

0x74BB–

0x74BC

29884–

29885

R

1

Hour

INT32U

0–4 294 967 295

A/E

Hours current was 80‑89% of nominal range

0x74BD–

0x74BE

29886–

29887

R

1

Hour

INT32U

0–4 294 967 295

A/E

Hours current was 90‑100% of nominal range

Temperature Profile Counters

The temperature profile counters report the number of hours for each range of temperature in the MicroLogic trip unit. If the temperature profile counters reach the maximum value 4 294 967 295 and a new temperature profile event occurs, then the temperature profile counters are reset to 0.

A read request of 12 registers is necessary to read the temperature profile counters.

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x74C1–

0x74C2

29890–

29891

R

1

Hour

INT32U

0–4 294 967 295

A/E

Hours temperature was < -30 °C (-22 °F)

0x74C3–

0x74C4

29892–

29893

R

1

Hour

INT32U

0–4 294 967 295

A/E

Hours temperature was in the -30–+59 °C range (22–1 38.2 °F)

0x74C5–

0x74C6

29894–

29895

R

1

Hour

INT32U

0–4 294 967 295

A/E

Hours temperature was in the +60–+74 °C range (140–165.2 °F)

0x74C7–

0x74C8

29896–

29897

R

1

Hour

INT32U

0–4 294 967 295

A/E

Hours temperature was in the +75–+89 °C range (167–192.2 °F)

0x74C9–

0x74CA

29898–

29899

R

1

Hour

INT32U

0–4 294 967 295

A/E

Hours temperature was in the +90–+99 °C range (194–210.2 °F)

0x74CB–

0x74CC

29900–

29901

R

1

Hour

INT32U

0–4 294 967 295

A/E

Hours temperature was > +100 °C (212 °F)

Protection Trips Counters

The protection trips counters report the number of protection trips for each type of protection: long-time, short-time, instantaneous, ground-fault, earth-leakage jam, unbalance, long-start, and underload protections.

The protection trips counters stop incrementing when they reach the maximum value 10000.

A read request of 9 registers is necessary to read the protection trips counters.

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x74D5

29910

R

1

–

INT16U

0–10000

A/E

Number of long-time protection trips

0x74D6

29911

R

1

–

INT16U

0–10000

A/E

Number of short-time protection trips

0x74D7

29912

R

1

–

INT16U

0–10000

A/E

Number of instantaneous protection trips

(including integrated instantaneous protection, instantaneous with earth-leakage protection, and reflex protection)

0x74D8

29913

R

1

–

INT16U

0–10000

A/E

Number of ground-fault protection trips

0x74D9

29914

R

1

–

INT16U

0–10000

E

Number of earth-leakage protection trips

0x74DA

29915

R

1

–

INT16U

0–10000

A/E

Number of jam protection trips

0x74DB

29916

R

1

–

INT16U

0–10000

A/E

Number of unbalance protection trips

0x74DC

29917

R

1

–

INT16U

0–10000

A/E

Number of long-start protection trips

0x74DD

29918

R

1

–

INT16U

0–10000

A/E

Number of underload protection trips

Alarms Counters

The alarms counters report the number of occurrences of the alarms. When an alarm is configured, the associated counter is set to 0. The alarm counters stop incrementing when they reach the maximum value 10000.

A read request of 13 registers is necessary to read the alarms counters.

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x74F3

29940

R

1

–

INT16U

0–10000

A/E

Counter of user-defined alarm 201

0x74F4

29941

R

1

–

INT16U

0–10000

A/E

Counter of user-defined alarm 202

0x74F5

29942

R

1

–

INT16U

0–10000

A/E

Counter of user-defined alarm 203

0x74F6

29943

R

1

–

INT16U

0–10000

A/E

Counter of user-defined alarm 204

0x74F7

29944

R

1

–

INT16U

0–10000

A/E

Counter of user-defined alarm 205

0x74F8

29945

R

1

–

INT16U

0–10000

A/E

Counter of user-defined alarm 206

0x74F9

29946

R

1

–

INT16U

0–10000

A/E

Counter of user-defined alarm 207

0x74FA

29947

R

1

–

INT16U

0–10000

A/E

Counter of user-defined alarm 208

0x74FB

29948

R

1

–

INT16U

0–10000

A/E

Counter of user-defined alarm 209

0x74FC

29949

R

1

–

INT16U

0–10000

A/E

Counter of user-defined alarm 210

0x74FD

29950

R

1

–

INT16U

0–10000

A/E

Counter of pre-alarm Ir

0x74FE

29951

R

1

–

INT16U

0–10000

A/E

Counter of pre-alarm Ig

0x74FF

29952

R

1

–

INT16U

0–10000

A/E

Counter of pre-alarm IΔn

Maintenance Operation Counters

The maintenance operation counters report the number of some maintenance operations. The maintenance operation counters stop incrementing when they reach the maximum value 10000.

A read request of 7 registers is necessary to read the maintenance operation counters.

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x751B

29980

R

1

–

INT16U

0–10000

A/E

Counter of MicroLogic trip unit locking pad activation

0x751C

29981

R

1

–

INT16U

0–10000

A/E

Counter of connections of the UTA maintenance module

0x751D

29982

R

1

–

INT16U

0–10000

A/E

Counter of ground-fault test operation (using MicroLogic keypad only)

0x751E

29983

R

1

–

INT16U

0–10000

E

Counter of earth-leakage test operation

0x751F

29984

R

1

–

INT16U

0–10000

A/E

Counter of ZSI (Zone Selective Interlocking) test operation

0x7520

29985

R

1

–

INT16U

0–10000

A/E

Counter of numerical injection test operation

0x7521

29986

R

1

–

INT16U

0–10000

A/E

Counter of reset Firmware command