DOCA0091EN-08

Event Commands

Acknowledge a Latched Output

The user can read the SDx module outputs parameters from register 9801 to 9810 Configuration of the SDx Module.

To acknowledge a latched output, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

–

–

INT16U

46216

A/E

Command code = 46216

0x1F40

8001

–

–

INT16U

12

A/E

Number of parameters (bytes) = 12

0x1F41

8002

–

–

INT16U

5121

A/E

Destination = 5121 (0x1401)

0x1F42

8003

–

–

INT16U

1

A/E

Security type of the command

0x1F43–

0x1F44

8004–

8005

–

–

OCTET STRING

–

A/E

Password of the command: Administrator or Operator user profile password

0x1F45

8006

–

–

INT16U

1–2

A/E

1 = relay 1, 2 = relay 2

Acknowledge a Trip

To acknowledge a trip, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

–

–

INT16U

46217

A/E

Command code = 46217

0x1F40

8001

–

–

INT16U

10

A/E

Number of parameters (bytes) = 10

0x1F41

8002

–

–

INT16U

5121

A/E

Destination = 5121 (0x1401)

0x1F42

8003

–

–

INT16U

1

A/E

Security type of the command

0x1F43–

0x1F44

8004–

8005

–

–

OCTET STRING

–

A/E

Password of the command: Administrator user profile password