DOCA0091EN-08

Time-Stamped Information

General Description

The time-stamped information enables the user to know all the dates relative to important information such as previous protection settings and minimum/maximum values of currents, voltages, and system frequency.

The time-stamped information table describes:

  • the previous protection setup parameters and corresponding dates

  • the minimum and maximum values of voltage measurements and corresponding dates

  • the maximum values of current measurements and corresponding dates

  • the minimum and maximum system frequencies and corresponding dates

  • the peak demand of current and power and corresponding dates

A read request of 100 registers is necessary to read the time-stamped previous protection registers (29600–29699).

Previous Long-Time Protection Setup

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x739F

29600

R

1

A

INT16U

–

A/E

Previous Ir pick-up value. The Ir range depends on the nominal current In.

0x73A0–

0x73A2

29601–

29603

R

–

–

ULP DATE

–

A/E

Date and time of the previous setup.

0x73A3

29604

R

1

ms

INT16U

500– 16000

A/E

Previous tr time delay (distribution application)

tr = 500, 1000, 2000, 4000, 8000, 16000 ms

0x73A4–

0x73A6

29605–

29607

R

–

–

ULP DATE

–

A/E

Date and time of the previous setup.

0x73A7

29608

R

1

–

INT16U

5–30

A/E

Motor class (motor application only)

Possible values = 5, 10, 20, 30 s

0x73A8–

0x73AA

29609–

29611

R

–

–

ULP DATE

–

A/E

Date and time of the previous setup.

0x73AB

29612

R

–

–

INT16U

1–2

A/E

Previous cool fan setup (motor application only)

1 = auto, 2 =motor

0x73AC–

0x73AE

29613–

29615

R

–

–

ULP DATE

–

A/E

Date and time of the previous setup.

Previous Short-Time Protection Setup

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x73AF

29616

R

10

–

INT16U

(1)

A/E

Previous Isd coefficient pick-up value

0x73B0–

0x73B2

29617–

29619

R

–

–

ULP DATE

–

A/E

Date and time of the previous setup.

0x73B3

29620

R

1

ms

INT16U

0–400

A/E

Previous tsd time delay

tsd = 0, 100, 200, 300, 400 ms

If tsd = 0 ms, then I2t must be Off.

0x73B4–

0x73B6

29621–

29623

R

–

–

ULP DATE

–

A/E

Date and time of the previous setup.

0x73B7

29624

R

–

–

INT16U

0–1

A/E

Previous type of protection: 0 = I2t On, 1 = I2t Off

0x73B8–

0x73BA

29625–

29627

R

–

–

ULP DATE

–

A/E

Date and time of the previous setup.

(1) The Isd coefficient range depends on:

  • the application:

    • for distribution application, the range is 15–100, adjustable in step of 5.

    • for motor application, the range is 50–130, adjustable in step of 5.

  • the MicroLogic trip unit rotary switch if it exists.

Previous Instantaneous Protection Setup

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x73BB

29628

R

10

–

INT16U

(1)

A/E

Previous Ii coefficient pick-up value

0x73BC–

0x73BE

29629–

29631

R

–

–

ULP DATE

–

A/E

Date and time of the previous setup.

(1) The Ii coefficient range depends on the circuit breaker size:

  • for 100–160 A, the range is 15–150.

  • for 250–400 A, the range is 15–120.

  • for 630 A, the range is 15–110.

Previous Ground-Fault Protection Setup

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x73BF

29632

R

100

ms

INT16U

(1)

A/E

Previous Ig coefficient pick-up value.

0x73C0–

0x73C2

29633–

29635

R

–

–

ULP DATE

–

A/E

Date and time of the previous setup.

0x73C3

29636

R

1

ms

INT16U

0–400

A/E

Previous tg time delay

tg = 0, 100, 200, 300, 400 ms

0x73C4–

0x73C6

29637–

29639

R

–

–

ULP DATE

–

A/E

Date and time of the previous setup.

0x73C7

29640

R

–

–

INT16U

0–1

A/E

Previous type of protection: 0 = I2t On, 1 = I2t Off

0x73C8–

0x73CA

29641–

29643

R

–

–

ULP DATE

–

A/E

Date and time of the previous setup.

(1) The Ig coefficient range depends on the nominal current In and the MicroLogic trip unit rotary switch if it exists.

For example, 0 (protection off) or 0.40 In to In in step of 0.05.

Previous Earth-Leakage Protection Setup

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x73CB

29644

R

1

mA

INT16U

–

E

Previous IΔn pick-up value. The IΔn depends on the nominal current In.

0x73CC–

0x73CE

29645–

29647

R

–

–

ULP DATE

–

E

Date and time of the previous setup.

0x73CF

29648

R

1

ms

INT16U

0–1000

E

Previous tΔn time delay

tΔn = 0, 60, 150, 500, 1000 ms

If IΔn = 0.03 mA, then TΔn = 0 ms.

0x73D0–

0x73D2

29649–

29651

R

–

–

ULP DATE

–

E

Date and time of the previous setup.

Previous Jam Protection Setup

The jam protection is available for motor application only.

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x73D3

29652

R

–

–

INT16U

0–2

E

Previous setup status: 0 = Off, 1 = On

0x73D4–

0x73D6

29653–

29655

R

–

–

ULP DATE

–

E

Date and time of the previous setup.

0x73D7

29656

R

10

–

INT16U

10–80

E

Previous Ijam coefficient pick-up value

0x73D8–

0x73DA

29657–

29659

R

–

–

ULP DATE

–

E

Date and time of the previous setup.

0x73DB

29660

R

1

s

INT16U

1–30

E

Previous tjam time delay

0x73DC–

0x73DE

29661–

29663

R

–

–

ULP DATE

–

E

Date and time of the previous setup.

Previous Unbalance Protection Setup

The unbalance protection is available for motor application only.

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x73DF

29664

R

1

%

INT16U

10–40

E

Previous unbalance coefficient pick-up value

0x73E0–

0x73E2

29665–

29667

R

–

–

ULP DATE

–

E

Date and time of the previous setup.

0x73E3

29668

R

1

s

INT16U

1–10

E

Previous tunbal time delay

0x73E4–

0x73E6

29669–

29671

R

–

–

ULP DATE

–

E

Date and time of the previous setup.

Previous Underload Protection Setup

The underload protection is available for motor application only.

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x73E7

29672

R

–

–

INT16U

0–2

E

Previous setup status: 0 = Off, 1 = On

0x73E8–

0x73EA

29673–

29675

R

–

–

ULP DATE

–

E

Date and time of the previous setup.

0x73EB

29676

R

100

–

INT16U

30–90

E

Previous Iunderload coefficient pick-up value

0x73EC–

0x73EE

29677–

29679

R

–

–

ULP DATE

–

E

Date and time of the previous setup.

0x73EF

29680

R

1

s

INT16U

1–200

E

Previous tunderload time delay

0x73F0–

0x73F2

29681–

29683

R

–

–

ULP DATE

–

E

Date and time of the previous setup.

Previous Long-Start Protection Setup

The long-start protection is available for motor application only.

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x73F3

29684

R

–

–

INT16U

0–2

E

Previous setup status: 0 = Off, 1 = On

0x73F4–

0x73F6

29685–

29687

R

–

–

ULP DATE

–

E

Date and time of the previous setup.

0x73F7

29688

R

10

–

INT16U

10–50

E

Previous Ilongstart coefficient pick-up value

0x73F8–

0x73FA

29689–

29691

R

–

–

ULP DATE

–

E

Date and time of the previous setup.

0x73FB

29692

R

1

s

INT16U

1–30

E

Previous tlongstart time delay

0x73FC–

0x73FE

29693–

29695

R

–

–

ULP DATE

–

E

Date and time of the previous setup.

Previous Neutral Protection Setup

The neutral protection is only available when system type in register 3314 is 30 or 41 System Type.

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x73FF

29696

R

–

–

INT16U

0–3

A/E

Previous neutral coefficient pick-up value:

0 = Off

1 = 0.5

2 = 1.0

3 = OSN

0x7400–

0x7402

29697–

29699

R

–

–

ULP DATE

–

A/E

Date and time of the previous setup.

Minimum/Maximum V12 Voltage Measurements

A read request of 48 registers is necessary to read the time-stamped minimum/maximum values of voltage, current, and frequency registers (29780–29827).

Register = 0 if voltage < 25 V.

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x7453

29780

R

1

V

INT16U

0–850

E

Minimum of RMS phase-to-phase voltage V12

0x7454–

0x7456

29781–

29783

R

–

–

ULP DATE

–

E

Date and time.

0x7457

29784

R

1

V

INT16U

0–850

E

Maximum of RMS phase-to-phase voltage V12

0x7458–

0x745A

29785–

29787

R

–

–

ULP DATE

–

E

Date and time.

Minimum/Maximum V23 Voltage Measurements

Register = 0 if voltage < 25 V.

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x745B

29788

R

1

V

INT16U

0–850

E

Minimum of RMS phase-to-phase voltage V23

0x745C–

0x745E

29789–

29791

R

–

–

ULP DATE

–

E

Date and time.

0x745F

29792

R

1

V

INT16U

0–850

E

Maximum of RMS phase-to-phase voltage V23

0x7460–

0x7462

29793–

29795

R

–

–

ULP DATE

–

E

Date and time.

Minimum/Maximum V31 Voltage Measurements

Register = 0 if voltage < 25 V.

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x7463

29796

R

1

V

INT16U

0–850

E

Minimum of RMS phase-to-phase voltage V31

0x7464–

0x7466

29797–

29799

R

–

–

ULP DATE

–

E

Date and time.

0x7467

29800

R

1

V

INT16U

0–850

E

Maximum of RMS phase-to-phase voltage V31

0x7468–

0x746A

29801–

29803

R

–

–

ULP DATE

–

E

Date and time.

Maximum I1 Current Measurement

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x746B

29804

R

1

A

INT16U

0–20xIn

A/E

Maximum of RMS current on phase 1: I1

0x746C–

0x746E

29805–

29807

R

–

–

ULP DATE

–

A/E

Date and time.

Maximum I2 Current Measurement

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x746F

29808

R

1

A

INT16U

0–20xIn

A/E

Maximum of RMS current on phase 2: I2

0x7470–

0x7472

29809–

29811

R

–

–

ULP DATE

–

A/E

Date and time.

Maximum I3 Current Measurement

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x7473

29812

R

1

A

INT16U

0–20xIn

A/E

Maximum of RMS current on phase 3: I3

0x7474–

0x7476

29813–

29815

R

–

–

ULP DATE

–

A/E

Date and time.

Maximum IN Current Measurement

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x7477

29816

R

1

A

INT16U

0–20xIn

A/E

Maximum of RMS current on neutral: IN

0x7478–

0x747A

29817–

29819

R

–

–

ULP DATE

–

A/E

Date and time.

Minimum System Frequency

When the MicroLogic trip unit cannot calculate the frequency, it returns Not Evaluated = 32768 (0x8000).

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x747B

29820

R

10

Hz

INT16U

150–4400

E

Minimum of system frequency

0x747C–

0x747E

29821–

29823

R

–

–

ULP DATE

–

E

Date and time.

Maximum System Frequency

When the MicroLogic trip unit cannot calculate the frequency, it returns Not Evaluated = 32768 (0x8000).

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x747F

29824

R

10

Hz

INT16U

150–4400

E

Maximum of system frequency

0x7480–

0x7482

29825–

29827

R

–

–

ULP DATE

–

E

Date and time.

I1 Peak Demand Measurement

A read request of 20 registers is necessary to read the time-stamped peak demand of current and power (29828–29847).

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x7483

29828

R

1

A

INT16U

0–20xIn

E

I1 peak demand

0x7484–

0x7486

29829–

29831

R

–

–

ULP DATE

–

E

Date and time.

I2 Peak Demand Measurement

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x7487

29832

R

1

A

INT16U

0–20xIn

E

I2 peak demand

0x7488–

0x748A

29833–

29835

R

–

–

ULP DATE

–

E

Date and time.

I3 Peak Demand Measurement

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x748B

29836

R

1

A

INT16U

0–20xIn

E

I3 peak demand

0x748C–

0x748E

29837–

29839

R

–

–

ULP DATE

–

E

Date and time.

IN Peak Demand Measurement

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x748F

29840

R

1

A

INT16U

0–20xIn

E

IN peak demand

0x7490–

0x7492

29841–

29843

R

–

–

ULP DATE

–

E

Date and time.

P Peak Demand Measurement

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x7493

29844

R

10

kW

INT16

-30000–

+30000

E

P peak demand

0x7494–

0x7496

29845–

29847

R

–

–

ULP DATE

–

E

Date and time.