990-91274J-001

Installation Procedure

NOTE: The distance between the battery bank and the UPS must not exceed 200 m. Contact Schneider Electric for installations with a longer distance.
  1. Perform one of the following:
  2. Connect the Power Cables.
  3. Final Installation.
For moving or decommissioning the classic battery cabinet after installation has been completed, please see Decommission or Move the Classic Battery Cabinet to a New Location.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.