990-6392E-001

Recommended Cable Sizes for Easy UPS 3-Phase Modular

DANGER
hazard of electric shock, explosion, or arc flash
All wiring must comply with all applicable national and/or electrical codes. The maximum allowable cable size is 185 mm².
Failure to follow these instructions will result in death or serious injury.

Cable sizes in this manual are based on table B.52.5 of IEC 60364-5-52 with the following assertions:

  • 90 °C conductors

  • An ambient temperature of 30 °C

  • Use of copper conductors (Tin)

  • Installation method C

PE size is based on table 54.2 of IEC 60364-4-54.

If the ambient temperature is greater than 30 °C, larger conductors are to be used in accordance with the correction factors of the IEC.

NOTE: Refer to the UPS installation manual for UPS input cable sizes.
    3+0 Parallel Capacity 2+0 Parallel Capacity
2+1 Parallel Redundant
1+0 Single
1+1 Parallel Redundant
UPS rating   Per Phase (mm²) Neutral (mm2) PE (mm²) Per Phase (mm²) Neutral (mm2) PE (mm²) Per Phase (mm²) Neutral (mm2) PE (mm²)
50 kW UPS output

16

2x16

16

16

2x16

16

16

2x16

16

Input (single mains)/
bypass (dual mains)

2x50

2x95

50

70

2x70

35

16

2x16

16

Load

2x50

2x95

50

70

2x70

35

16

2x16

16

100 kW UPS output

70

2x70

35

70

2x70

35

70

2x70

35

Input (single mains)/
bypass (dual mains)

4x50

4x95

120

2x70

4x70

70

70

2x70

35

Load

4x50

4x95

120

2x70

4x70

70

70

2x70

35

150 kW UPS output

120

120

70

120

120

70

Input (single mains)/
bypass (dual mains)

4x50

4x95

120

120

120

70

Load

4x50

4x95

120

120

120

70

200 kW UPS output

2x70

2x70

70

2x70

2x70

70

Input (single mains)/
bypass (dual mains)

4x70

4x70

185

2x70

2x70

70

Load

4x70

4x70

185

2x70

2x70

70

250 kW UPS output

2x95

2x95

95

Input (single mains)/
bypass (dual mains)

2x95

2x95

95

Load

2x95

2x95

95

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.