0000509775_02_en

Additional Placement Information for EcoStruxure Battery Management System Modules with External Temperature Sensors

For EcoStruxure Battery Management System modules with external temperature sensors: Make sure that the temperature sensor is placed at the same position on each battery.

NOTE: The cable for the temperature sensor is 23 cm (9 inches) or 90 cm (35 inches) long.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.