0000509775_02_en

Attach the EcoStruxure Battery Management System Modules

To attach the EcoStruxure Battery Management System modules on the batteries:
  1. Remove the adhesive film from the fastening strips. Each module has two strips.
  2. Position the module over the correct placement.
  3. Press down and hold the module under moderate pressure for 5-10 seconds.
  4. Check that the module is securely fixed on the battery.
  5. Connect the measuring cable plug to the socket at the bottom of the module.
    NOTE: The measuring cable is equipped with a mechanical protection against accidental polarity reversal.

Example of EcoStruxure Battery Management System Module Installation

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.