0000509775_02_en

Standards and Certificates

Directives and Regulations

2014/30/EU Electromagnetic compatibility - directive

2011/65/EU and (EU) 2015/863 Restriction of the use of certain hazardous substances (RoHS)

2012/19/EU Waste electrical and electronic equipment (WEEE)

2006/66/EG Waste Batteries and accumulators and repealing directive

CE Conformity

EN 55024:2010
Information technology equipment - Immunity characteristics - Limits and methods of measurement

EN 55022:2003
Information technology equipment - Radio disturbance characteristics - Limits and methods of measurement

EN 55032:2015
Electromagnetic compatibility of multimedia equipment - Emission - Limits and methods of measurement

EN 61000-4-3:2006+A1:2008+A2:2010
Electromagnetic compatibility (EMC) Part 4: Environment Section 3: Radiated, radio-frequency, electromagnetic field immunity test. Limits and methods of measurement

IEC 61010-1:2010
General safety requirements for the following types of electrical equipment and their accessories, wherever they are intended to be used. A) Electrical test and measurement equipment B) Electrical industrial process-control equipment C) Electrical laboratory equipment

EN IEC 63000:2018
Technical documentation for the assessment of electrical and electronic products with respect to the restriction of hazardous substances; European version

EN 62368-1:2014 + AC:2015
Information Technology Equipment – Safety

UL/CSA Certification

NOTE: Currently only certain devices are UL/CSA certified, for details refer to the section Technical Data.

UL Std. No. 60950-1 2nd Edition
Information Technology Equipment – Safety – Part 1: General Requirements (Incl. AM 1:2011 and AM 2:2014)

CAN/CSA-C22.2 No. 60950-1-07
Incl. Amendment 1 (2011) and Amendment 2 (2014) - Information Technology Equipment – Safety – Part 1: General Requirements

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.