0000509775_02_en

Communication

From the webmanager it is possible to receive different events and alarms via Modbus and SNMP.

To change the Modbus or SNMP settings:

  1. Make sure the network settings are correctly configured for your network, see Network Settings.

  2. Navigate to Services > Modbus or Services > SNMP Agent from the side menu.

  3. Make necessary settings and changes for your network setup.

    IMPORTANT: Make sure that the Modbus or SNMP settings confirm to your cyber security policy.
  4. Click Apply to confirm any changes.

For the mapping lists see:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.