0000509775_02_en

Find a Module with a Specific Address

NOTE: The programmer mode in the programmer page must be toggled On to find the address of a single module or to program a single module.

From the programmer page:

  1. Under the Module section, in the Address field enter the module address you want to find.

  2. Click Show.

  3. The status LED on the module with the entered address will start to flash red and green.

    NOTE: The LED will continue to flash until the module button is pressed with the pen.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.