0000509775_02_en

General Placement Information

The recommended placement is on top of the battery.

If there is not enough space on the top of the battery, place the EcoStruxure Battery Management System module on the front panel of the battery.

NOTICE
hazard of gas condensate dripping into the connection
  • Pace the modules with the measuring cables in a loop with the connection pointing down.
  • Check that any original battery auxiliary (for example, a plastic cover) is reinstalled after the modules are placed.
Failure to follow these instructions can result in equipment damage.

Avoid placing the EcoStruxure Battery Management System modules on any cooling ribs or plugs.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.