0000509775_02_en

Initial Local Connection to the Webmanager

First login with default IP address:

  1. Check that the webmanager slide switch is in the left position.

  2. Connect your workstation to the webmanagers LAN port with an Ethernet cable, directly or through a switch.

  3. On your workstation run Command Prompt as administrator.

  4. In the Command Prompt window type route add 10.10.10.10 xxx.xxx.xxx.xxx, where xxx.xxx.xxx.xxx is the local IP of your workstation.

  5. Press Enter. A success confirmation will be shown in the Command Prompt window.

  6. Open a web browser from your workstation.

  7. Enter https://10.10.10.10 in the browser address field. A login window will open.

  8. In the login window enter:

    • User: admin
    • Password: cs141-snmp
    NOTE: After the first log in the user is prompted and required to set a new password.

  9. The first login will run the System Setup Wizard that will help you setup the basic configurations of the webmanager.

    NOTE: If the System Setup Wizard does not start automatically on the first login you can launch it by clicking System > Wizard

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.