0000509775_02_en

Install the Webmanager and any Splitting Boxes

Before attaching the bus cables:

  • Consider what bus cable lengths to use, the cables are available in multiple lengths to avoid unnecessary cable length.

  • Check the information and maximum distances for the bus cable installation in the chapter Bus Cable Length and Wiring Details.

  • If a repeater is needed because the maximum distance is exceeded, install the repeater less than 100 m (328 ft) from the webmanager. The maximum distances are then calculated from the repeater instead of the webmanager.

  1. Mount the webmanager or the control cabinet with the webmanager inside.
  2. If applicable, mount the splitting box(es).
  3. Only for solutions without splitting box(es):
    1. Attach the bus cable (A) from the closest module to the webmanager.
    2. Attach the power supply cable (C) to the webmanager.
    IMPORTANT: Always use a secure power source as the power supply to the webmanager.
  4. Only for solutions with splitting box(es):
    1. Attach the bus cable(s) (A) from the closest module(s) to the splitting box(es).
    2. If applicable, attach the bus cables (A) between any additional splitting boxes.
    3. Attach the bus cable (B) from the closest splitting box to the webmanager.
    4. Attach the power supply cable (C) to the webmanager.
    IMPORTANT: Always use a secure power source as the power supply to the webmanager.

Examples of Webmanager and Splitting Box Installations

Example Installation with Splitting Box

Example Installation without Splitting Box

Example Installations with Control Cabinets

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.