0000509775_02_en

Install Battery Measuring Cables

CAUTION
INACCURATE MEASUREMENTS
Make sure to tighten the pole screws with the correct torque value for your battery.
Failure to follow these instructions can result in injury or equipment damage.
NOTICE
Always connect the measuring cable to the right pole, the red cable to the positive pole and the black cable to the negative pole. If the cable connection is reversed the integrated fuse can be damaged.
Failure to follow these instructions can result in equipment damage.

Follow the procedure to connect the measuring cable for your battery type using the right cable:

NOTE: Please refer to the battery manufacturers connection guidelines for resistance/impedance measurements.

4 V – 16 V Batteries 1.2 V - 2 V Batteries with 2 poles 1.2 V - 2 V Batteries with 4 poles or more
BC5xx measuring cable BC4Bxx measuring cable
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.