0000509775_02_en

SNMP OID List

There are several object identifiers (OID) available from the EcoStruxure Battery Management System webmanager via SNMP. The webmanager SNMP access needs to be configured. To view and change the SNMP settings from the web interface navigate to Services > SNMP Agent.

The MIB file can be downloaded from: www.se.com.

NOTE: Some read values have a scale factor. The read value needs to be multiplied with the scale facture to get the correct value for the unit of measure.

Settings OIDs

NOTE: The bacsSettings shows configured settings and alarm thresholds for the setup. The table bacsSettings lists a mix of read only and read-write OIDs. All other tables only contain read only OIDs.

OID Address: 1.3.6.1.2.1.33.5.1 / OID Name: bacsSettings

OID Address OID Name Description
(read only / read-write)
Scale [Unit] Example of Read Value*
1.3.6.1.2.1.33.5.1.1 bacsModuleType Module Type. 0 = C20, 1 = C21, 10 = C30, 20 = C40, 20 = C41.
(read only)
1 c20(0) -> Module type C20
1.3.6.1.2.1.33.5.1.2 bacsNumStrings Number of battery strings.
(read only)
1 2
1.3.6.1.2.1.33.5.1.3 bacsNumBatteries Total number of batteries.
(read only)
1 18
1.3.6.1.2.1.33.5.1.4 bacsBattCap Capacity of installed batteries.
(read only)
1 [Ah] 50
1.3.6.1.2.1.33.5.1.5 bacsLogRate1 The configured period between log recordings during normal operation. Period between log recordings.
(read only)
1 [s] 1200 -> 1200 seconds (20 minutes)*
1.3.6.1.2.1.33.5.1.6 bacsLogRate2 The configured period between log recordings during charge or discharge.
(read only)
1 [s] (The readings are done as soon as possible.)*
1.3.6.1.2.1.33.5.1.7 bacsImpcPollRate The configured period between internal impedance polls.
(read-write)
1 [min] 720 -> 720 minutes (12 hours)*
1.3.6.1.2.1.33.5.1.8 bacsImpcLowAlarm Impedance low alarm level.
(read-write)
0.01 [mΩ] 110 -> 1.1 mΩ
1.3.6.1.2.1.33.5.1.9 bacsImpcHighAlarm Impedance high alarm level.
(read-write)
1 5000 -> 50 mΩ
1.3.6.1.2.1.33.5.1.10 bacsTemperatureLowAlarm Temperature alarm below this level.
(read-write)
0.1 [C° or F°]* 50 -> 5 C°
1.3.6.1.2.1.33.5.1.11 bacsTemperatureHighAlarm Temperature alarm above this level.
(read-write)
0.1 [C° or F°]* 350 -> 35 C°
1.3.6.1.2.1.33.5.1.12 bacsVoltageLowAlarm Voltage alarm below this level.
(read-write)
0.01 [V] 1200 -> 12 V
1.3.6.1.2.1.33.5.1.13 bacsVoltageHighAlarm Voltage alarm above this level.
(read-write)
0.01 [V] 1550 -> 15.5 V
1.3.6.1.2.1.33.5.1.14 bacsImpcLowWarn Impedance low warning level.
(read-write)
0.01 [mΩ] 120 -> 1.2 mΩ
1.3.6.1.2.1.33.5.1.15 bacsImpcHighWarn Impedance high warning level.
(read-write)
0.01 [mΩ] 4000 -> 40 mΩ
1.3.6.1.2.1.33.5.1.16 bacsTemperatureLowWarn Temperature warning below this level.
(read-write)
0.1 [C° or F°]* 100 -> 10 C°
1.3.6.1.2.1.33.5.1.17 bacsTemperatureHighWarn Temperature warning above this level.
(read-write)
0.1 [C° or F°]* 300 -> 30 C°
1.3.6.1.2.1.33.5.1.18 bacsVoltageLowWarn Voltage warning below this level.
(read-write)
0.01 [V] 1200 -> 12 V
1.3.6.1.2.1.33.5.1.19 bacsVoltageHighWarn Voltage warning above this level.
(read-write)
0.01 [V] 1410 -> 14.1 V
1.3.6.1.2.1.33.5.1.20 bacsTemperatureUnit Temperature unit currently in use. 0 = Celsius, 1 = Fahrenheit.
(read-write)
1 Celsius(0)
1.3.6.1.2.1.33.5.1.21 bacsStringVoltageLowAlarm The configured alarm threshold for the battery string voltage low alarm.
(read-write)
0.01 [V] 10500 -> 105 V
1.3.6.1.2.1.33.5.1.22 bacsStringVoltageHighAlarm The configured alarm threshold for the battery string voltage high alarm.
(read-write)
0.01 [V] 13500 -> 135 V
1.3.6.1.2.1.33.5.1.23 bacsStringVoltageLowWarn The configured alarm threshold for the battery string voltage low warning.
(read-write)
0.01 [V] 11000 -> 110 V
1.3.6.1.2.1.33.5.1.24 bacsStringVoltageHighWarn The configured alarm threshold for the battery string voltage high warning.
(read-write)
0.01 [V] 12500 -> 125 V
1.3.6.1.2.1.33.5.1.25 bacsStringCurrentDeviationDischargeAlarm The configured alarm threshold for the current difference between the battery strings alarm.
(read-write)
0.01 [A] 1000 -> 10 A
1.3.6.1.2.1.33.5.1.26 bacsStringCurrentDeviationChargeAlarm The configured alarm threshold for the charge current difference between the battery strings alarm.
(read-write)
0.01 [A] 1000 -> 10 A
1.3.6.1.2.1.33.5.1.27 bacsStringCurrentDeviationDischargeWarn The configured warning threshold for the charge current difference between the battery strings warning.
(read-write)
0.01 [A] 500 -> 5 A
1.3.6.1.2.1.33.5.1.28 bacsStringCurrentDeviationChargeWarn The configured warning threshold for the charge current difference between the battery warning.
(read-write)
0.01 [A] 500 -> 5 A

Objects OIDs

OID Address: 1.3.6.1.2.1.33.5.2 / OID Name: bacsObjects

OID Address OID Name Description Scale [Unit] Example of Read Value
1.3.6.1.2.1.33.5.2.1 bacsStatus EcoStruxure Battery Management System status flags. For information about the flags see General Status Flags Description. (Decimal format) 65 -> 0x0041
1.3.6.1.2.1.33.5.2.2 bacsAvModuleVolt Average module voltage. 0.01 [V] 1287 -> 12.87 V
1.3.6.1.2.1.33.5.2.3 bacsTotalVolt Total voltage of all modules. 0.01 [V] 23176 -> 231.76 V
1.3.6.1.2.1.33.5.2.4 bacsNumModules The number of installed battery modules. 1 18
1.3.6.1.2.1.33.5.2.5 bacsModuleTable The list of battery table entries. N/A N/A
1.3.6.1.2.1.33.5.2.5.1 bacsModuleEntry An entry containing information applicable to a particular battery. N/A N/A
1.3.6.1.2.1.33.5.2.5.1.1 bacsModuleIndex The module identifier. 1
  • bacsModuleIndex.1: 0
  • bacsModuleIndex.2: 1
  • ….
1.3.6.1.2.1.33.5.2.5.1.2 bacsModuleVoltage Ordered list of the measured battery voltage by each module. 0.01 [V]
  • bacsModuleVoltage.1: 1290
  • bacsModuleVoltage.2: 1288
  • ….
1.3.6.1.2.1.33.5.2.5.1.3 bacsModuleTemperature Ordered list of the temperature measured by each module. 0.1 [C° or F°]*
  • bacsModuleTemperature.1: 270
  • bacsModuleTemperature.2: 270
  • ….
1.3.6.1.2.1.33.5.2.5.1.4 bacsModuleBypass Ordered list of the module bypass measured by each module. 0.1 [%]
  • bacsModuleBypass.1: 0
  • bacsModuleBypass.2: 0
  • ….
1.3.6.1.2.1.33.5.2.5.1.5 bacsModuleResistance Ordered list of the measured module impedance in each module. 0.01 [mΩ]
  • bacsModuleResistance.1: 468
  • bacsModuleResistance.2: 471
  • ….
1.3.6.1.2.1.33.5.2.5.1.6 bacsModuleState The general module alarm flags. For information about the flags see Alarm Flags Description. (Decimal format)
  • bacsModuleState.1: 0
  • bacsModuleState.2: 0
  • ….
(0 -> 0x0000)
1.3.6.1.2.1.33.5.2.6 bacsNumStrings The number of installed battery strings. 1 2
1.3.6.1.2.1.33.5.2.7 bacsStringTable The list of stringy table entries. N/A N/A
1.3.6.1.2.1.33.5.2.7.1 bacsStringEntry An entry that contains information about a specific string of batteries. N/A N/A
1.3.6.1.2.1.33.5.2.7.1.1 bacsStringIndex The string identifier. 1
  • bacsStringIndex.1: 0
  • bacsStringIndex.2: 1
  • ….
1.3.6.1.2.1.33.5.2.7.1.2 bacsStringCurrent The string current. 0.01 [A]
  • bacsStringCurrent.1: 0
  • bacsStringCurrent.2: 0
  • ….
1.3.6.1.2.1.33.5.2.7.1.3 bacsStringTotalVolt The string total voltage. 0.01 [V]
  • bacsStringTotalVolt.1: 11497
  • bacsStringTotalVolt.2: 11438
  • ….
1.3.6.1.2.1.33.5.2.7.1.4 bacsStringAverageVol The string average voltage per battery. 0.01 [V]
  • bacsStringAverageVol.1: 1277
  • bacsStringAverageVol.2: 1270
  • ….
1.3.6.1.2.1.33.5.2.7.1.5 bacsStringCurrentAC The string AC current. 0.01 [A]
  • bacsStringCurrentAC.1: 0
  • bacsStringCurrentAC.2: 0
  • ….
1.3.6.1.2.1.33.5.2.7.1.6 bacsStringAlarm The general string alarm flags. For information about the flags see Alarm Flags Description. (Decimal format)
  • bacsStringAlarm.1: 0
  • bacsStringAlarm.2: 0
  • ….
(0 -> 0x0000)
1.3.6.1.2.1.33.5.2.7.1.7 bacsStringAlarm2 The string alarm flags. For information about the flags see Battery String Alarm Flags Description. (Decimal format)
  • bacsStringAlarm2.1: 0
  • bacsStringAlarm2.2: 0
  • ….
(0 -> 0x0000)

Alarm OIDs

OID Address: 1.3.6.1.2.1.33.5.3 / OID Name: bacsAlarms

OID Address OID Name Description
1.3.6.1.2.1.33.5.3.1 bacsAlarmsPresent The present number of active alarm conditions.
1.3.6.1.2.1.33.5.3.2 bacsAlarmTable A list of alarm entries.
1.3.6.1.2.1.33.5.3.2.1 bacsAlarmEntry An entry containing information applicable to a particular alarm.
1.3.6.1.2.1.33.5.3.2.1.1 bacsAlarmId A unique identifier for an alarm condition. This value must remain constant.
1.3.6.1.2.1.33.5.3.2.1.2 bacsAlarmDescr A reference to an alarm description object. The object referenced should not be accessible, but rather be used to provide a unique description of the alarm condition.
1.3.6.1.2.1.33.5.3.2.1.3 bacsAlarmTime The value of sysUpTime when the alarm condition was detected. If the alarm condition was detected during the webmanager startup and presumably existed before the webmanager startup, then dcAlarmTime = 0.
1.3.6.1.2.1.33.5.3.3 bacsWellKnownAlarms A list of traps, see Alarm Trap List.
1.3.6.1.2.1.33.5.3.4 bacsModuleAlarmsPresent The number of EcoStruxure Battery Management System modules currently in an alarm state.
1.3.6.1.2.1.33.5.3.5 bacsModuleWarningsPresent The number of EcoStruxure Battery Management System modules currently in a warning state.

Alarm Trap List

NOTE: Make sure a trap receiver is correctly configured to receive notification when the trap is active.

OID Address (SNMP Traps): 1.3.6.1.2.1.33.5.3.3 / OID Name: bacsWellKnownAlarms

OID Address OID Name Description
1.3.6.1.2.1.33.5.3.3.1 bacsAlarmSystemError This object indicates a communication problem from the webmanager to one or more of the battery modules.
1.3.6.1.2.1.33.5.3.3.2 bacsAlarmResistWarn This object indicates that the internal resistance of one or more batteries is above the warning level.
1.3.6.1.2.1.33.5.3.3.3 bacsAlarmResistAlarm This object indicates that the internal resistance of one or more batteries is above the alarm level.
1.3.6.1.2.1.33.5.3.3.4 bacsAlarmVoltage This object indicates that the voltage of one or more batteries is outside the defined rage.
1.3.6.1.2.1.33.5.3.3.5 bacsAlarmTemperature This object indicates that the temperature of one or more batteries is outside the defined range.
1.3.6.1.2.1.33.5.3.3.6 bacsAlarmVoltageHigh This object indicates that the voltage of one or more batteries is higher than the defined range.
1.3.6.1.2.1.33.5.3.3.7 bacsAlarmVoltageLow This object indicates that the voltage of one or more batteries is lower than the defined range.
1.3.6.1.2.1.33.5.3.3.8 bacsAlarmTemperatureHigh This object indicates that the temperature of one or more batteries is higher than the defined range.
1.3.6.1.2.1.33.5.3.3.9 bacsAlarmTemperatureLow This object indicates that the temperature of one or more batteries is lower than the defined range.
1.3.6.1.2.1.33.5.3.3.10 bacsAlarmResistAlarmHigh This object indicates that the internal resistance of one or more batteries is above the alarm level.
1.3.6.1.2.1.33.5.3.3.11 bacsAlarmResistAlarmLow This object indicates that the internal resistance of one or more batteries is below the alarm level.
1.3.6.1.2.1.33.5.3.3.12 bacsAlarmEqualizing This object indicates that the equalizing is not operating correctly.
1.3.6.1.2.1.33.5.3.3.13 bacsAlarmVoltageWarnHigh This object indicates that the voltage of one or more batteries is higher than the defined warning range.
1.3.6.1.2.1.33.5.3.3.14 bacsAlarmVoltageWarnLow This object indicates that the voltage of one or more batteries is lower than the defined warning range.
1.3.6.1.2.1.33.5.3.3.15 bacsAlarmTemperatureWarnHigh This object indicates that the temperature of one or more batteries is higher than the defined warning range.
1.3.6.1.2.1.33.5.3.3.16 bacsAlarmTemperatureWarnLow This object indicates that the temperature of one or more batteries is lower than the defined warning range.
1.3.6.1.2.1.33.5.3.3.17 bacsAlarmResistWarnHigh This object indicates that the internal resistance of one or more batteries is higher than the defined warning range.
1.3.6.1.2.1.33.5.3.3.18 bacsAlarmResistWarnLow This object indicates that the internal resistance of one or more batteries is lower than the defined warning range.
1.3.6.1.2.1.33.5.3.3.19 bacsAlarmInitializing The webmanager is initializing.
1.3.6.1.2.1.33.5.3.3.20 bacsAlarmCommunicationLost BACS bus communication is lost.
1.3.6.1.2.1.33.5.3.3.21 bacsAlarmBatteryBreakerOpen Battery breaker is open.
1.3.6.1.2.1.33.5.3.3.22 bacsAlarmThermalRunaway Thermal runaway detected.
1.3.6.1.2.1.33.5.3.3.23 bacsAlarmSensorCommunicationLost Sensor communication is lost.
1.3.6.1.2.1.33.5.3.3.24 bacsAlarmDischarging Batteries are being discharged.
1.3.6.1.2.1.33.5.3.3.25 bacsAlarmDischargingStopped Batteries are no longer being discharged.
1.3.6.1.2.1.33.5.3.3.26 bacsAlarmMaxVoltageDiff The voltage difference is too high.
1.3.6.1.2.1.33.5.3.3.27 bacsAlarmStringVoltHigh The battery string voltage is above the configured alarm threshold.
1.3.6.1.2.1.33.5.3.3.28 bacsAlarmStringVoltLow The battery string voltage is below the configured alarm threshold.
1.3.6.1.2.1.33.5.3.3.29 bacsAlarmStringVoltHighWarn The battery string voltage is above the configured warning threshold.
1.3.6.1.2.1.33.5.3.3.30 bacsAlarmStringVoltLowWarn The battery string voltage is below the configured warning threshold.
1.3.6.1.2.1.33.5.3.3.31 bacsAlarmStringCurrentHigh The battery string current is above the configured alarm threshold.
1.3.6.1.2.1.33.5.3.3.32 bacsAlarmStringCurrentLow The battery string current is below the configured alarm threshold.
1.3.6.1.2.1.33.5.3.3.33 bacsAlarmStringCurrentHighWarn The battery string current is above the configured warning threshold.
1.3.6.1.2.1.33.5.3.3.34 bacsAlarmStringCurrentLowWarn The battery string current is below the configured warning threshold.
1.3.6.1.2.1.33.5.3.3.35 bacsAlarmStringEqualizingDisabled The battery string equalizing is disabled.
1.3.6.1.2.1.33.5.3.3.36 bacsAlarmStringCurrDeviationCharge The charge current difference between the battery strings is above the configured alarm threshold.
1.3.6.1.2.1.33.5.3.3.37 bacsAlarmStringCurrDeviationDischarge The discharge current difference between the battery strings is above the configured alarm threshold.
1.3.6.1.2.1.33.5.3.3.38 bacsAlarmStringCurrDeviationChargeWarn The charge current difference between the battery strings is above the configured warning threshold.
1.3.6.1.2.1.33.5.3.3.39 bacsAlarmStringCurrDeviationDischargeWarn The discharge current difference between the battery strings is above the configured warning threshold.

Traps OIDs

NOTE: Make sure a trap receiver is correctly configured to receive notification when the trap is active.

OID Address (SNMP Traps): 1.3.6.1.2.1.33.5.4 / OID Name: bacsTraps

OID Address OID Name Description
1.3.6.1.2.1.33.5.4.1 bacsTrapAlarmEntryAdded Sent when an alarm in the system appears.
1.3.6.1.2.1.33.5.4.2 bacsTrapAlarmEntryRemoved Sent when an alarm in the system disappears.

GX_R_AUX OIDs

NOTE: In gxRAUX the input OIDs can have the status normal or alarm. The output OIDs can have the status on or off.

OID Address: 1.3.6.1.2.1.33.5.5 / OID Name: gxRAUX

OID Address OID Name Description Example of Read Value
1.3.6.1.2.1.33.5.5.1 gxRAUX1Input1 Status of input 1 on GX_R_AUX 1. normal ( 1 )
1.3.6.1.2.1.33.5.5.2 gxRAUX1Input2 Status of input 2 on GX_R_AUX 1. normal ( 1 )
1.3.6.1.2.1.33.5.5.3 gxRAUX1Input3 Status of input 3 on GX_R_AUX 1. normal ( 1 )
1.3.6.1.2.1.33.5.5.4 gxRAUX1Input4 Status of input 4 on GX_R_AUX 1. normal ( 1 )
1.3.6.1.2.1.33.5.5.5 gxRAUX1Output1 Status of output 1 on GX_R_AUX 1. off ( 0 )
1.3.6.1.2.1.33.5.5.6 gxRAUX1Output2 Status of output 2 on GX_R_AUX 1. off ( 0 )
1.3.6.1.2.1.33.5.5.7 gxRAUX1Output3 Status of output 3 on GX_R_AUX 1. off ( 0 )
1.3.6.1.2.1.33.5.5.8 gxRAUX1Output4 Status of output 4 on GX_R_AUX 1. off ( 0 )
1.3.6.1.2.1.33.5.5.9 gxRAUX2Input1 Status of input 1 on GX_R_AUX 2. normal ( 1 )
1.3.6.1.2.1.33.5.5.10 gxRAUX2Input2 Status of input 2 on GX_R_AUX 2. normal ( 1 )
1.3.6.1.2.1.33.5.5.11 gxRAUX2Input3 Status of input 3 on GX_R_AUX 2. normal ( 1 )
1.3.6.1.2.1.33.5.5.12 gxRAUX2Input4 Status of input 4 on GX_R_AUX 2. normal ( 1 )
1.3.6.1.2.1.33.5.5.13 gxRAUX2Output1 Status of output 1 on GX_R_AUX 2. off ( 0 )
1.3.6.1.2.1.33.5.5.14 gxRAUX2Output2 Status of output 2 on GX_R_AUX 2. off ( 0 )
1.3.6.1.2.1.33.5.5.15 gxRAUX2Output3 Status of output 3 on GX_R_AUX 2. off ( 0 )
1.3.6.1.2.1.33.5.5.16 gxRAUX2Output4 Status of output 4 on GX_R_AUX 2. off ( 0 )
1.3.6.1.2.1.33.5.5.17 gxRAUX3Input1 Status of input 1 on GX_R_AUX 3. normal ( 1 )
1.3.6.1.2.1.33.5.5.18 gxRAUX3Input2 Status of input 2 on GX_R_AUX 3. normal ( 1 )
1.3.6.1.2.1.33.5.5.19 gxRAUX3Input3 Status of input 3 on GX_R_AUX 3. normal ( 1 )
1.3.6.1.2.1.33.5.5.20 gxRAUX3Input4 Status of input 4 on GX_R_AUX 3. normal ( 1 )
1.3.6.1.2.1.33.5.5.21 gxRAUX3Output1 Status of output 1 on GX_R_AUX 3. off ( 0 )
1.3.6.1.2.1.33.5.5.22 gxRAUX3Output2 Status of output 2 on GX_R_AUX 3. off ( 0 )
1.3.6.1.2.1.33.5.5.23 gxRAUX3Output3 Status of output 3 on GX_R_AUX 3. off ( 0 )
1.3.6.1.2.1.33.5.5.24 gxRAUX3Output4 Status of output 4 on GX_R_AUX 3. off ( 0 )
1.3.6.1.2.1.33.5.5.25 gxRAUX4Input1 Status of input 1 on GX_R_AUX 4. normal ( 1 )
1.3.6.1.2.1.33.5.5.26 gxRAUX4Input2 Status of input 2 on GX_R_AUX 4. normal ( 1 )
1.3.6.1.2.1.33.5.5.27 gxRAUX4Input3 Status of input 3 on GX_R_AUX 4. normal ( 1 )
1.3.6.1.2.1.33.5.5.28 gxRAUX4Input4 Status of input 4 on GX_R_AUX 4. normal ( 1 )
1.3.6.1.2.1.33.5.5.29 gxRAUX4Output1 Status of output 1 on GX_R_AUX 4. off ( 0 )
1.3.6.1.2.1.33.5.5.30 gxRAUX4Output2 Status of output 2 on GX_R_AUX 4. off ( 0 )
1.3.6.1.2.1.33.5.5.31 gxRAUX4Output3 Status of output 3 on GX_R_AUX 4. off ( 0 )
1.3.6.1.2.1.33.5.5.32 gxRAUX4Output4 Status of output 4 on GX_R_AUX 4. off ( 0 )
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.