0000509775_02_en

Configure Modules from the Programmer

NOTE
To program the modules the slider on the programmer page needs to be toggled to On. This activates programmer mode and stops the bus polling. After the module addresses have been programmed toggle the slider to Off to deactivate programmer mode and go to operation mode.

The integrated programmer is used to configure the modules. Navigate to Devices > BACS > Programmer from the side menu to access the programmer page.

From the programmer page it is possible to:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.