DOCA0248EN-21

Major Fixes for Version 002.002.000

The following bugs are fixed in Panel Server firmware version 002.002.000:

  • Modbus devices associated with a custom model and supporting only Function code 04 were displayed as Not connected in the Panel Server after upgrading the Panel Server to firmware version 002.000.000.

  • Energy meters in the iEM2050 family displayed unstable connected/disconnected status in Panel Server webpages.

  • Connection to a hidden network was not supported.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.