DOCA0248EN-19

Firmware Version 001.006.000

New Features

  • I/O Smart Link (reference A9XMSB11): full support of commissioning and control function of the device outputs by using Panel Server webpages.

  • Addition of wireless devices:

    • PowerTag Control: commissioning by using Panel Server webpages or EcoStruxure Power Commission software.

    • PowerLogic PD100 partial discharge monitoring sensor: commissioning by using Panel Server webpages.

  • PowerTag Control digital input settings: predefined contextualization values. For example, Fan status is available when configuring the status of an IO device connected to either one of the input of the PowerTag Control 2DI wireless device, or the input or output of a PowerTag Control IO wireless device.

  • Enhancement of Panel Server features for EcoStruxure Asset Advisor and EcoStruxure Resource Advisor:

    • Panel Server supports additional enhancements for custom model properties, by using EPC-Web software:

      • Additional option for properties: LogicCode.

      • Byte ordering at measurement level.

    • PowerLogic HeatTag enhancements.

    • Modbus TCP/IP and Modbus serial devices on unit ID 248 to 254.

    • Panel Server supports custom alarms in custom models created in EPC-Web software.

General Features

The following table presents the availability of general features on Panel Server Advanced in firmware version 001.006.000.

Available

Not available

General features

Availability

Functionality

Separated network topology

Switched network topology

Connection to Edge Control (EcoStruxure Power Monitoring Expert, EcoStruxure Power Operation,EcoStruxure Building Operation, any Building Management System, or third-party monitoring or supervision system)

Ability to disable concurrently and permanently the wireless networks (Wi-Fi and IEEE 802.15.4) by using Panel Server webpages

Wi-Fi

2.4 GHz

5 GHz

External Wi-Fi antenna (reference: PASA-ANT1)

IEEE 802.15.4 communication

Maximum number of wireless devices:

  • Up to 40 wireless devices as combination of PowerTag Energy sensors, PowerLogic Tag energy sensors, Acti9 Active, wireless indication auxiliaries for ComPacT and PowerPacT circuit breakers, wireless CO2 sensors, wireless temperature and humidity sensors, PowerTag A, PowerTag Ambient, Easergy TH110/CL110 environmental sensors, and PowerLogic HeatTag sensors, PowerTag Control, and PowerLogic PD100 with maximum 10 PowerTag Control devices, maximum 15 PowerLogic HeatTag, and maximum 15 PowerLogic PD100 sensors

  • or up to 85 Easergy TH110/CL110 environmental sensors

NOTE: Total number of PowerTag Control, PowerLogic HeatTag, and PowerLogic PD100 should not exceed 20 devices.

Modbus TCP/IP communication

64 Modbus TCP/IP devices maximum including devices physically connected to the Panel Server and virtual devices (that is, IEEE 802.15.4 devices connected to a child Panel Server gateway)

Human Machine Interface (HMI)

FDM128 Ethernet display

PowerTag Link display

Backup restore

Backup and Panel Server configuration restore by using Panel Server webpages and EcoStruxure Power Commission software

Configuration

User management by single user account

User management by multiple users with Role-Based Access Control (RBAC)

Alarms

  • In general, publication of alarms supported by the end devices.

  • Publication of alarms related to:

    • Communication issue between a device and Panel Server when available from the end devices

    • ERMS on circuit breaker

    • The three levels of alarms from HeatTag sensors

Protocols

Modbus TCP/IP server

Modbus TCP/IP client

DHCP client

DHCP server

DPWS server

HTTPS

SFTP client

Data export

Panel Server webpages for publication on SFTP server

Publication on Schneider Electric cloud by using Panel Server webpages

CSV export on PC by using Panel Server webpages

Commissioning and Monitoring Features

The following table presents the availability of commissioning and monitoring features on Panel Server Advanced in firmware version 001.006.000.

Available

Not available

Commissioning and monitoring features

Availability

Modbus serial communication

Commissioning of feature to use the Modbus serial port in reverse mode by using Panel Server webpages

Digital inputs (PAS800L)

Commissioning by using EcoStruxure Power Commission software

Commissioning by using Panel Server webpages

Monitoring by using EcoStruxure Power Commission software

Monitoring by using Panel Server webpages

Status assignment from a list of predefined values for each generic input/output in the IO status setting by using EcoStruxure Power Commission software or Panel Server webpages

Firmware update

Applied to one Panel Server gateway by using EcoStruxure Power Commission software

Applied to one Panel Server gateway by using Panel Server webpages

Applied to several Panel Server gateways by using EcoStruxure Power Commission software

Applied to several Panel Server gateways by using Panel Server webpages

Backup restore

Backup restore on a Panel Server of the same model by using EcoStruxure Power Commission software

Backup restore on a Panel Server of the same model by using Panel Server webpages

Configuration

Configuration by using EcoStruxure Power Commission software

Ethernet configuration for upstream communication by using Panel Server webpages

Modbus configuration of Modbus TCP/IP and Modbus serial devices by using Panel Server webpages

Selective pairing of wireless devices by using EcoStruxure Power Commission software

Selective pairing of wireless devices by using Panel Server webpages

Disable concurrently and permanently the wireless networks (Wi-Fi and IEEE 802.15.4) in the Panel Server by using Panel Server webpages

Monitoring

Display of data of I/O Smart Link devices by using Panel Server webpages

Display of data of Panel Server digital inputs by using Panel Server webpages

Display of data of the supported devices (see commercial references in Supported Devices) by using Panel Server webpages

Diagnostic by using Panel Server webpages

Email notification

Email notification of selected alarms by using EcoStruxure Power Commission software

Email notification of selected alarms by using Panel Server webpages

Data logging

Access to 3-year data logger with predefined data sampling that can be configured by using Panel Server webpages

Access to 3-year data logger with predefined data sampling with EcoStruxure Power Commission software

Performance and Limitations

  • Performance and limitations on Panel Server Advanced:

    • When SFTP publication is enabled, alarms are displayed in the Panel Server webpages but are not published on SFTP Server.

    • No manual addition of wireless devices connected to a child/downstream gateway by using EcoStruxure Power Commission software.

    • Automatic discovery of wireless devices under a child gateway is limited to 64 devices because wireless devices are seen as Modbus TCP/IP devices.

    • The typical response time to Modbus TCP/IP request for a wireless IEEE 802.15.4 device is 30 ms.

    • The maximum response time to Modbus TCP/IP request for a wireless IEEE 802.15.4 device is 1 s, set up Modbus/TCP client timeout accordingly.

    • Typical Panel Server latency between Modbus TCP/IP request forwarded to the Modbus serial network is 10 ms.

    • Wi-Fi function available through a connection to a Wi-Fi infrastructure only. Access point function not available.

  • Limitations on logging and alarming:

    • The number of individual data points that can be sampled is limited to 2,000 and limited to a flow of 500 data points per minute.

    • The number of individual alarms that can be configured for monitoring and sending an email notification is limited to 100.

  • Limitations on I/O Smart Link:

    • I/O contextualization (IO status setting in EcoStruxure Power Commission software or Panel Server webpages) is not available.

    • Circuit breaker status is not published in case of selection of Wired Devices family.

    • Signal Element as predefined Standard I/O is not available.

    • No predefined configuration is available for Schneider Electric pulse counters.

    • Neither operating time, nor operation counter, nor trip counter for Wired devices and Standard I/O.

  • Limitations on wireless devices:

    • PowerTag Control:

      • Feedback loop in contactor mode is not supported.

      • Configuration in impulse relay mode is not supported.

      • If a PowerTag Control device is connected to a child gateway:

        • No automatic discovery.

        • No data is published to the parent gateway. To be able to publish at the parent gateway level, a custom model has to be developed for the parent gateway.

        • No control function is available through the Panel Server webpages.

      • Pairing process to be followed:

        1. Pair the PowerTag Control devices if any in the configuration (all the other wireless devices must be unpowered).

        2. Pair the PowerLogic HeatTag sensors if any in the configuration.

        3. Pair PowerLogic PD100 if any in the configuration.

        4. Pair the other wireless devices.

    • PowerTag Display: not supported by Panel Server Advanced.

  • Limitations on topology publication to the Schneider Electric cloud: all the devices must be connected at least once to the Panel Server to enable the correct topology to be published to the Schneider Electric cloud.

  • Limitations on custom model for wireless devices connected under a child gateway: if a custom model uses the same name as a predefined model and devices are already associated with the predefined model, follow this procedure to load the custom model:

    1. Decommission any device already associated with the predefined model.

    2. Load the custom model in the Panel Server.

    3. Reboot the Panel Server.

    4. Associate the devices with the newly loaded custom model.

    5. Publish the topology in case of use of the Panel Server with a Schneider Electric cloud application such EcoStruxure Asset Advisor or EcoStruxure Resource Advisor.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.