DOCA0172EN-20

Configuration of PowerTag Control Devices Through Webpages

Presentation

PowerTag Control devices can be configured through Panel Server webpages.

Configuration Procedure

To configure PowerTag Control devices follow the procedure in Configuring Wireless Devices Through Webpages.

Parameter Tables

Identification

Refer to Configuring Wireless Devices Through Webpages.

Communication Settings

Parameter name Description

Communication period (s)

When available for the selected wireless device, you can set the communication period at a value different from the value set at family devices level. Select a value of between 5 and 120 seconds from the list.

Modbus virtual

Refer to Configuring Wireless Devices Through Webpages.

Input/Output Settings

Parameter name Description

Local Control

Toggles local control on or off.

IMPORTANT: When Local Control is disabled, no manual control is possible on the device.

Configuration Type

Select from the list:

  • Contactor without feedback loop: Configure parameters for Output and Input separately

  • Contactor with feedback loop

  • Impulse relay

The parameters displayed depend on the selection of configuration type. See details in the following tables.

Parameters for Contactor without feedback loop

Parameter name Description

Output

I/O Type

Select from the list:

  • Standard I/O

  • Not connected

Name

Enter the name of the wireless device.

Label

Enter the label of the wireless device (optional).

I/O Contextualization

Select an option from the list.

Status name

If you select Custom as contextualization option, then enter the custom name for the device.

Meaning of output = 0

Displayed values depend on selection of I/O Contextualization. Enter your custom values if you select Custom as contextualization option.

NOTE: Clicking the double arrow icon on the right allows you to swap the meanings of outputs 0 and 1.

Meaning of output = 1

Displayed values depend on selection of I/O Contextualization. Enter your custom values if you select Custom as contextualization option.

NOTE: Clicking the double arrow icon on the right allows you to swap the meanings of outputs 0 and 1.

Commodity

Select the commodity to be monitored from the list.

Usage

Select the usage to be monitored from the list.

Zone

Select the zone in the list, as contextualization data.

Click the Settings icon to:

  • Create a new zone

  • Modify a zone name

  • Delete a zone

For more information about creating, modifying and deleting zones, refer to Zone Management.

Input

I/O Type

Select from the list:

  • Standard I/O

  • Not connected

Name

Enter the name of the wireless device.

Label

Enter the label of the wireless device (optional).

I/O Contextualization

Select an option from the list.

Meaning of output = 0

Engaged (for display only).

NOTE: Clicking the double arrow icon on the right allows you to swap the meanings of outputs 0 and 1.

Meaning of output = 1

Released (for display only).

NOTE: Clicking the double arrow icon on the right allows you to swap the meanings of outputs 0 and 1.

Commodity

Select the commodity to be monitored from the list.

Usage

Select the usage to be monitored from the list.

Zone

Select the zone in the list, as contextualization data.

Click the Settings icon to:

  • Create a new zone

  • Modify a zone name

  • Delete a zone

For more information about creating, modifying and deleting zones, refer to Zone Management.

Parameters for Contactor with feedback loop and for Impulse Relay

Parameter name Description

I/O Type

Select from the list:

  • Standard I/O

  • Not connected

    NOTE: No parameters are displayed if Not connected is selected.

Output/Input Feedback Loop

Name

Enter the name of the wireless device.

Label

Enter the label of the wireless device (optional).

Commodity

Select the commodity to be monitored from the list.

Usage

Select the usage to be monitored from the list.

Zone

Select the zone in the list, as contextualization data.

Click the Settings icon to:

  • Create a new zone

  • Modify a zone name

  • Delete a zone

For more information about creating, modifying and deleting zones, refer to Zone Management.

I/O Contextualization

Select an option from the list.

Status name

If you select Custom as contextualization option, then enter the custom name for the device.

Meaning of output = 0

Displayed values depend on selection of I/O Contextualization. Enter your custom values if you select Custom as contextualization option.

NOTE: Clicking the double arrow icon on the right allows you to swap the meanings of outputs 0 and 1.

Meaning of output = 1

Displayed values depend on selection of I/O Contextualization. Enter your custom values if you select Custom as contextualization option.

NOTE: Clicking the double arrow icon on the right allows you to swap the meanings of outputs 0 and 1.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.