DOCA0172EN-21

Custom model

A device model created by the user, which defines the list of measurements and alarms supported by the Modbus device connected to the Panel Server. The custom model can be for a device for which no built-in model exists, or for a device where a built-in model exists but only a limited list of measurements and alarms are required by the user. The custom model is created using the EPC Web tool.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.