DOCA0172EN-21

Proxy

Presentation

It is necessary to configure proxy settings in the Panel Server when both the following conditions are met:

  • if you use the remote access or cloud connection, and

  • if your network administrator has implemented a proxy on your local network.

The proxy address and port number are provided by your network administrator.

Availability

This function is available on Panel Server Entry, Universal, and Advanced.

Setting the Parameters

Proxy is set on the Panel Server webpages, at Settings > Network communication > Proxy.

Proxy Activation Settings

Parameter Description

HTTP proxy

Used to enable/disable the HTTP proxy (disabled by default).

HTTPS proxy

Used to enable/disable the HTTPS proxy (disabled by default).

HTTP and HTTPS Proxy Settings

The following parameters are displayed only when the parameter HTTP proxy or HTTPS proxy is enabled.

Parameter Description

Address

Used to enter the IP address or domain name of the HTTP or HHTPS proxy server.

IMPORTANT: Do not type prefix http:// or https://.

Port

Used to enter the HTTP or HHTPS port.

Authentication

Used to enable/disable if proxy authentication is required (disabled by default).

Non-proxy hosts

Used to enter the exceptions of hosts in a non-proxy host list.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.