DOCA0172EN-21

Appendix C: Wireless Device Network Indicators

Network Indicators

The following table describes the network indicators of wireless devices.

Information type Description

RSSI (received signal strength indicator)

Displays the power level of the wireless signal:

  • 0 to -75 dBm indicates a good power level.

  • -75 to -85 dBm indicates an average power level.

  • ≤ -85 dBm indicates a poor power level with risk of outage.

LQI (link quality indicator)

Displays the measurement of the strength and/or the quality of the received frames.

PER (packet error rate)

Displays the ratio of the number of packets which do not reach a destination over the total expected number of packets. It is expressed as a percentage.

The calculation of the PER (packet error rate) indicator depends on the type of indicator:

  • Device indicator: provided by the device.

  • Panel Server indicator: calculated over a sliding window equal to 20 x publication period, and refreshed every 30 seconds.

  • Link indicator: displays the higher of the two previous indicators.

Signal Quality Level

  • PER Link indicator:
    The PER link indicator is based on the PER of the Panel Server and the PER of the device as explained in the following table:

  PER of the device

PER < 20% or no device PER

20% ≤ PER < 30%

30% ≤ PER

PER of Panel Server

PER < 10%

Low

Medium

High

10% ≤ PER < 15%

Medium

Medium

High

15% ≤ PER

High

High

High

  • Signal quality level:
    The signal quality level is based on the PER link indicator and RSSI as explained in the following table:

  RSSI

RSSI > -75 dBm

-85 dBm < RSSI ≤ -75 dBm

RSSI ≤ -85 dBm

PER link indicator

Low

Excellent

Excellent

Good

Medium

Good

Good

Fair

High

Fair

Weak

Weak

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.